SketchEllipseBuilder Class¶
-
class
NXOpen.
SketchEllipseBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.SketchEllipseBuilder
builderTo create a new instance of this class, use
NXOpen.SketchCollection.CreateSketchEllipseBuilder
Default values.
Property Value Closed true EndAngle.Value 360 MajorRadius.Value 50 (millimeters part), 2 (inches part) MinorRadius.Value 25 (millimeters part), 1 (inches part) RotationAngle.Value 0 StartAngle.Value 0 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
CenterPoint | Returns or sets the center point |
Closed | Returns or sets the closed flag |
EndAngle | Returns the end angle |
MajorPoint | Returns or sets the point in major axis to calculate the major radius |
MajorRadius | Returns the major radius |
MinorPoint | Returns or sets the point in minor axis to calculate the minor radius |
MinorRadius | Returns the minor radius |
RotationAngle | Returns the rotation angle |
StartAngle | Returns the start angle |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
HandleComplement | Adjust the constraints and dimensions on ellipse vertices when we want to complement the ellipse |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CenterPoint¶
-
SketchEllipseBuilder.
CenterPoint
¶ Returns or sets the center point
-------------------------------------
Getter Method
Signature
CenterPoint()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CenterPoint(centerPoint)
Parameters: centerPoint ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: None.
Closed¶
-
SketchEllipseBuilder.
Closed
¶ Returns or sets the closed flag
-------------------------------------
Getter Method
Signature
Closed()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Closed(closed)
Parameters: closed (bool) – New in version NX6.0.0.
License requirements: None.
EndAngle¶
-
SketchEllipseBuilder.
EndAngle
¶ Returns the end angle
-------------------------------------
Getter Method
Signature
EndAngle()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
MajorPoint¶
-
SketchEllipseBuilder.
MajorPoint
¶ Returns or sets the point in major axis to calculate the major radius
-------------------------------------
Getter Method
Signature
MajorPoint()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MajorPoint(majorPoint)
Parameters: majorPoint ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: None.
MajorRadius¶
-
SketchEllipseBuilder.
MajorRadius
¶ Returns the major radius
-------------------------------------
Getter Method
Signature
MajorRadius()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
MinorPoint¶
-
SketchEllipseBuilder.
MinorPoint
¶ Returns or sets the point in minor axis to calculate the minor radius
-------------------------------------
Getter Method
Signature
MinorPoint()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinorPoint(minorPoint)
Parameters: minorPoint ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: None.
MinorRadius¶
-
SketchEllipseBuilder.
MinorRadius
¶ Returns the minor radius
-------------------------------------
Getter Method
Signature
MinorRadius()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
RotationAngle¶
-
SketchEllipseBuilder.
RotationAngle
¶ Returns the rotation angle
-------------------------------------
Getter Method
Signature
RotationAngle()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
StartAngle¶
-
SketchEllipseBuilder.
StartAngle
¶ Returns the start angle
-------------------------------------
Getter Method
Signature
StartAngle()
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
Method Detail¶
HandleComplement¶
-
SketchEllipseBuilder.
HandleComplement
¶ Adjust the constraints and dimensions on ellipse vertices when we want to complement the ellipse
Signature
HandleComplement()
New in version NX10.0.0.
License requirements: None.
Validate¶
-
SketchEllipseBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.