SketchDimensionGeometry_Struct Struct¶
NXOpen.Sketch.DimensionGeometry is an alias for NXOpen.SketchDimensionGeometry_Struct
-
class
NXOpen.
SketchDimensionGeometry_Struct
¶ Bases:
object
Used in the dimension creation methods to indicate what geometry to create the dimension on.
<code> Examples: 1. To specify the start point of line1 Geometry = line1 AssocType = StartPoint AssocValue = 0 </code>
Fields¶
Field | Description |
---|---|
Geometry | |
AssocType | |
AssocValue | See table for meaning. |
HelpPoint | help point |
View | The view the geometry is dependent on, if any |
Geometry¶
-
SketchDimensionGeometry_Struct.
Geometry
¶ -------------------------------------
Getter Method Signature
Geometry()
Returns: Return type: NXOpen.NXObject
-------------------------------------
Setter Method
Signature
Geometry(value)
Parameters: value ( NXOpen.NXObject
) –
AssocType¶
-
SketchDimensionGeometry_Struct.
AssocType
¶ -------------------------------------
Getter Method Signature
AssocType()
Returns: Return type: NXOpen.SketchAssocType
-------------------------------------
Setter Method
Signature
AssocType(value)
Parameters: value ( NXOpen.SketchAssocType
) –
AssocValue¶
-
SketchDimensionGeometry_Struct.
AssocValue
¶ See table for meaning.
<code> The AssocValue has the following meanings: AssocType AssocValue meaning ———- ——————- Tangency parameter percentage (0 - 100) (used to find approximate tangent point) CurvePoint the index number of the defining point of the spline(starting from 1) all else not used </code>
-------------------------------------
Getter Method Signature
AssocValue()
Returns: Return type: int -------------------------------------
Setter Method
Signature
AssocValue(value)
Parameters: value (int) –
HelpPoint¶
-
SketchDimensionGeometry_Struct.
HelpPoint
¶ help point
-------------------------------------
Getter Method Signature
HelpPoint()
Returns: Return type: NXOpen.Point3d
-------------------------------------
Setter Method
Signature
HelpPoint(value)
Parameters: value ( NXOpen.Point3d
) –
View¶
-
SketchDimensionGeometry_Struct.
View
¶ The view the geometry is dependent on, if any
-------------------------------------
Getter Method Signature
View()
Returns: Return type: NXOpen.NXObject
-------------------------------------
Setter Method
Signature
View(value)
Parameters: value ( NXOpen.NXObject
) –