SketchCopyObjectData_Struct Struct¶
NXOpen.Sketch.CopyObjectData is an alias for NXOpen.SketchCopyObjectData_Struct
-
class
NXOpen.
SketchCopyObjectData_Struct
¶ Bases:
object
This structure represents a map between the original object to be copied and the corresponding copied object.
An array of these structures are returned from the API
NXOpen.Sketch.CopyObjects
.
Fields¶
Field | Description |
---|---|
OrigObject | |
CopiedObject |
OrigObject¶
-
SketchCopyObjectData_Struct.
OrigObject
¶ -------------------------------------
Getter Method Signature
OrigObject()
Returns: Return type: NXOpen.NXObject
-------------------------------------
Setter Method
Signature
OrigObject(value)
Parameters: value ( NXOpen.NXObject
) –
CopiedObject¶
-
SketchCopyObjectData_Struct.
CopiedObject
¶ -------------------------------------
Getter Method Signature
CopiedObject()
Returns: Return type: NXOpen.NXObject
-------------------------------------
Setter Method
Signature
CopiedObject(value)
Parameters: value ( NXOpen.NXObject
) –