SketchConstraintGeometry_Struct Struct¶
NXOpen.Sketch.ConstraintGeometry is an alias for NXOpen.SketchConstraintGeometry_Struct
-
class
NXOpen.
SketchConstraintGeometry_Struct
¶ Bases:
object
Used by the create geometric constraint methods to indicate what geometry the constraint should be applied to.
<code> Examples:
Assume in these examples that you have a Line object in a variable named line1 and a Spline object in a variable named spline1.
1. To specify an entire line, set Geometry = line1 PointType = None SplineDefiningPointIndex = 0
2. To specify the start vertex of a line, set Geometry = line1 PointType = StartVertex SplineDefiningPointIndex = 0
3. To specify the third defining point of a spline Geometry = spline1 PointType = SplingDefiningPoint SplineDefiningPointIndex = 3
4. To specify the first defining point of a spline Geometry = spline1 PointType = StartVertex SplineDefiningPointIndex = 0 – OR – Geometry = spline1 PointType = SplingDefiningPoint SplineDefiningPointIndex = 1
Notes on splines: - spline defining points are numbered starting from 1 - to specify the first [or last] defining point of a spline, you can either use PointType = SplineDefiningPoint and set SplineDefiningPointIndex or use PointType = StartVertex [or EndVertex] - SplineDefiningPointIndex is only used when PointType = SplineDefiningPoint </code>
Fields¶
Field | Description |
---|---|
Geometry | |
PointType | |
SplineDefiningPointIndex | Ignored unless PointType is SplineDefiningPoint. |
Geometry¶
-
SketchConstraintGeometry_Struct.
Geometry
¶ -------------------------------------
Getter Method Signature
Geometry()
Returns: Return type: NXOpen.NXObject
-------------------------------------
Setter Method
Signature
Geometry(value)
Parameters: value ( NXOpen.NXObject
) –
PointType¶
-
SketchConstraintGeometry_Struct.
PointType
¶ -------------------------------------
Getter Method Signature
PointType()
Returns: Return type: NXOpen.SketchConstraintPointType
-------------------------------------
Setter Method
Signature
PointType(value)
Parameters: value ( NXOpen.SketchConstraintPointType
) –
SplineDefiningPointIndex¶
-
SketchConstraintGeometry_Struct.
SplineDefiningPointIndex
¶ Ignored unless PointType is SplineDefiningPoint.
Spline control points are numbered starting from 1
-------------------------------------
Getter Method Signature
SplineDefiningPointIndex()
Returns: Return type: int -------------------------------------
Setter Method
Signature
SplineDefiningPointIndex(value)
Parameters: value (int) –