SketchConstraintGeometryHelp_Struct Struct¶
NXOpen.Sketch.ConstraintGeometryHelp is an alias for NXOpen.SketchConstraintGeometryHelp_Struct
-
class
NXOpen.
SketchConstraintGeometryHelp_Struct
¶ Bases:
object
Used by several constraint creation methods that need a help point or parameter to indicate how to create the constraint.
The manner that the help point is used depends on the type of constraint
Fields¶
Field | Description |
---|---|
Type | Point or Parameter |
Point | Ignored unless type is Point |
Parameter | Ignored unless type is Parameter. |
Type¶
-
SketchConstraintGeometryHelp_Struct.
Type
¶ Point or Parameter
-------------------------------------
Getter Method Signature
Type()
Returns: Return type: NXOpen.SketchConstraintGeometryHelpType
-------------------------------------
Setter Method
Signature
Type(value)
Parameters: value ( NXOpen.SketchConstraintGeometryHelpType
) –
Point¶
-
SketchConstraintGeometryHelp_Struct.
Point
¶ Ignored unless type is Point
-------------------------------------
Getter Method Signature
Point()
Returns: Return type: NXOpen.Point3d
-------------------------------------
Setter Method
Signature
Point(value)
Parameters: value ( NXOpen.Point3d
) –
Parameter¶
-
SketchConstraintGeometryHelp_Struct.
Parameter
¶ Ignored unless type is Parameter.
Represents a parameter, typically along a curve
-------------------------------------
Getter Method Signature
Parameter()
Returns: Return type: float -------------------------------------
Setter Method
Signature
Parameter(value)
Parameters: value (float) –