SketchConstraintBuilderConstraint Enumeration¶
NXOpen.SketchConstraintBuilder.Constraint is an alias for NXOpen.SketchConstraintBuilderConstraint
-
class
NXOpen.
SketchConstraintBuilderConstraint
¶ Bases:
object
the types of the constraint
Enum Members
Enum Member Enum Member Description Coincident PointOnCurve Tangent Parallel Perpendicular Horizontal Vertical Midpoint Collinear Concentric EqualLength EqualRadius Symmetric Fixed FullyFixed ConstantAngle ConstantLength PointOnString NonUniformScale UniformScale SlopeOfCurve -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-