SketchConicBuilder Class¶
-
class
NXOpen.
SketchConicBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.SketchConicBuilder
builderTo create a new instance of this class, use
NXOpen.SketchCollection.CreateSketchConicBuilder
Default values.
Property Value Rho 0.5 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ControlPoint | Returns or sets the control point |
EndPoint | Returns or sets the end point |
Rho | Returns or sets the Rho value |
StartPoint | Returns or sets the start point |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ControlPoint¶
-
SketchConicBuilder.
ControlPoint
¶ Returns or sets the control point
-------------------------------------
Getter Method
Signature
ControlPoint()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ControlPoint(controlPoint)
Parameters: controlPoint ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: None.
EndPoint¶
-
SketchConicBuilder.
EndPoint
¶ Returns or sets the end point
-------------------------------------
Getter Method
Signature
EndPoint()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndPoint(endPoint)
Parameters: endPoint ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: None.
Rho¶
-
SketchConicBuilder.
Rho
¶ Returns or sets the Rho value
-------------------------------------
Getter Method
Signature
Rho()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Rho(rho)
Parameters: rho (float) – New in version NX6.0.0.
License requirements: None.
StartPoint¶
-
SketchConicBuilder.
StartPoint
¶ Returns or sets the start point
-------------------------------------
Getter Method
Signature
StartPoint()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartPoint(startPoint)
Parameters: startPoint ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
SketchConicBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.