SketchAlongPathBuilder Class¶
-
class
NXOpen.
SketchAlongPathBuilder
¶ Bases:
NXOpen.Builder
Use the
NXOpen.SketchAlongPathBuilder
to create or reattach aNXOpen.Sketch
along a path.To create a new instance of this class, use
NXOpen.SketchCollection.CreateSketchAlongPathBuilder
Default values.
Property Value ShowAllDatumAxes True SketchOrient Automatic New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Axis | Returns the horizontal reference |
NextThroughPointSolution | Returns the parameter indicating the location of the next solution |
OrientingFace | Returns the orienting faces to evaluate X and Y axis of sketch if NXOpen.SketchAlongPathBuilderSketchOrientationType is NXOpen.SketchAlongPathBuilderSketchOrientationType.RelativeToFace . |
PlaneLocation | Returns the plane location |
PlaneOrientation | Returns or sets the plane orientation type |
PlaneOrientationAxis | Returns or sets the plane orientation axis for one of the types of Normal to Vector, Parallel to Vector and Through Axis |
ReverseAxis | Returns or sets the flag to indicate the horizontal reference axis is reversed |
ReversePlaneNormal | Returns or sets the flag to indicate the plane normal is reversed |
Section | Returns the path |
ShowAllDatumAxes | Returns or sets the flag to create all datum axes for path having shared edge. |
SketchOrient | Returns or sets the sketch orientation method as NXOpen.SketchAlongPathBuilderSketchOrientationType |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SketchAlongPathBuilderPlaneOrientationType Enumeration | Indicates the orientation of the plane |
SketchAlongPathBuilderSketchOrientationType Enumeration | Indicates the sketch orientation method. |
Property Detail¶
Axis¶
-
SketchAlongPathBuilder.
Axis
¶ Returns the horizontal reference
-------------------------------------
Getter Method
Signature
Axis()
Returns: The sketch horizontal reference (X-axis) Return type: NXOpen.SelectIReferenceAxis
New in version NX5.0.0.
License requirements: None.
NextThroughPointSolution¶
-
SketchAlongPathBuilder.
NextThroughPointSolution
¶ Returns the parameter indicating the location of the next solution
-------------------------------------
Getter Method
Signature
NextThroughPointSolution()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
OrientingFace¶
-
SketchAlongPathBuilder.
OrientingFace
¶ Returns the orienting faces to evaluate X and Y axis of sketch if
NXOpen.SketchAlongPathBuilderSketchOrientationType
isNXOpen.SketchAlongPathBuilderSketchOrientationType.RelativeToFace
.The datum axes are evaluated as tangent and normal of the orienting face.
-------------------------------------
Getter Method
Signature
OrientingFace()
Returns: Return type: NXOpen.ScCollector
New in version NX6.0.0.
License requirements: None.
PlaneLocation¶
-
SketchAlongPathBuilder.
PlaneLocation
¶ Returns the plane location
-------------------------------------
Getter Method
Signature
PlaneLocation()
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX5.0.0.
License requirements: None.
PlaneOrientation¶
-
SketchAlongPathBuilder.
PlaneOrientation
¶ Returns or sets the plane orientation type
-------------------------------------
Getter Method
Signature
PlaneOrientation()
Returns: Return type: NXOpen.SketchAlongPathBuilderPlaneOrientationType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlaneOrientation(planeOrientationType)
Parameters: planeOrientationType ( NXOpen.SketchAlongPathBuilderPlaneOrientationType
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
PlaneOrientationAxis¶
-
SketchAlongPathBuilder.
PlaneOrientationAxis
¶ Returns or sets the plane orientation axis for one of the types of “Normal to Vector”, “Parallel to Vector” and “Through Axis”
-------------------------------------
Getter Method
Signature
PlaneOrientationAxis()
Returns: The plane orientation axis Return type: NXOpen.Direction
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlaneOrientationAxis(vector)
Parameters: vector ( NXOpen.Direction
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
ReverseAxis¶
-
SketchAlongPathBuilder.
ReverseAxis
¶ Returns or sets the flag to indicate the horizontal reference axis is reversed
-------------------------------------
Getter Method
Signature
ReverseAxis()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseAxis(reverseAxis)
Parameters: reverseAxis (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
ReversePlaneNormal¶
-
SketchAlongPathBuilder.
ReversePlaneNormal
¶ Returns or sets the flag to indicate the plane normal is reversed
-------------------------------------
Getter Method
Signature
ReversePlaneNormal()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReversePlaneNormal(reversePlaneNormal)
Parameters: reversePlaneNormal (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
Section¶
-
SketchAlongPathBuilder.
Section
¶ Returns the path
-------------------------------------
Getter Method
Signature
Section()
Returns: Return type: NXOpen.Section
New in version NX5.0.0.
License requirements: None.
ShowAllDatumAxes¶
-
SketchAlongPathBuilder.
ShowAllDatumAxes
¶ Returns or sets the flag to create all datum axes for path having shared edge.
This option is applicable only when
NXOpen.SketchAlongPathBuilderSketchOrientationType
isNXOpen.SketchAlongPathBuilderSketchOrientationType.RelativeToFace
-------------------------------------
Getter Method
Signature
ShowAllDatumAxes()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowAllDatumAxes(showAllDatumAxes)
Parameters: showAllDatumAxes (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
SketchOrient¶
-
SketchAlongPathBuilder.
SketchOrient
¶ Returns or sets the sketch orientation method as
NXOpen.SketchAlongPathBuilderSketchOrientationType
-------------------------------------
Getter Method
Signature
SketchOrient()
Returns: Return type: NXOpen.SketchAlongPathBuilderSketchOrientationType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SketchOrient(sketchOrientMethod)
Parameters: sketchOrientMethod ( NXOpen.SketchAlongPathBuilderSketchOrientationType
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
Method Detail¶
Validate¶
-
SketchAlongPathBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.