FlatPatternSettingsFlatPatternObjectTypeDisplay_Struct Struct¶
NXOpen.SheetMetal.FlatPatternSettings.FlatPatternObjectTypeDisplay is an alias for NXOpen.SheetMetal.FlatPatternSettingsFlatPatternObjectTypeDisplay_Struct
-
class
NXOpen.SheetMetal.
FlatPatternSettingsFlatPatternObjectTypeDisplay_Struct
¶ Bases:
object
The members of the following structure are the display data for an object in a flat pattern drawing member view.
Fields¶
Field | Description |
---|---|
Type | Object type |
IsEnabled | Enabled status for the object type |
Color | Object color |
Font | Object font |
Width | Object width |
Type¶
-
FlatPatternSettingsFlatPatternObjectTypeDisplay_Struct.
Type
¶ Object type
-------------------------------------
Getter Method Signature
Type()
Returns: Return type: NXOpen.SheetMetal.FlatPatternSettingsFlatPatternObjectType
-------------------------------------
Setter Method
Signature
Type(value)
Parameters: value ( NXOpen.SheetMetal.FlatPatternSettingsFlatPatternObjectType
) –
IsEnabled¶
-
FlatPatternSettingsFlatPatternObjectTypeDisplay_Struct.
IsEnabled
¶ Enabled status for the object type
-------------------------------------
Getter Method Signature
IsEnabled()
Returns: Return type: int -------------------------------------
Setter Method
Signature
IsEnabled(value)
Parameters: value (int) –
Color¶
-
FlatPatternSettingsFlatPatternObjectTypeDisplay_Struct.
Color
¶ Object color
-------------------------------------
Getter Method Signature
Color()
Returns: Return type: Id -------------------------------------
Setter Method
Signature
Color(value)
Parameters: value (Id) –
Font¶
-
FlatPatternSettingsFlatPatternObjectTypeDisplay_Struct.
Font
¶ Object font
-------------------------------------
Getter Method Signature
Font()
Returns: Return type: NXOpen.ViewDependentDisplayManagerFont
-------------------------------------
Setter Method
Signature
Font(value)
Parameters: value ( NXOpen.ViewDependentDisplayManagerFont
) –
Width¶
-
FlatPatternSettingsFlatPatternObjectTypeDisplay_Struct.
Width
¶ Object width
-------------------------------------
Getter Method Signature
Width()
Returns: Return type: NXOpen.ViewDependentDisplayManagerWidth
-------------------------------------
Setter Method
Signature
Width(value)
Parameters: value ( NXOpen.ViewDependentDisplayManagerWidth
) –