ShapeSearchBuilderOpenPartType Enumeration¶
NXOpen.ShapeSearch.ShapeSearchBuilder.OpenPartType is an alias for NXOpen.ShapeSearch.ShapeSearchBuilderOpenPartType
-
class
NXOpen.ShapeSearch.
ShapeSearchBuilderOpenPartType
¶ Bases:
object
The open part type enum
Enum Members
Enum Member Enum Member Description NotSetDisplayPart Not set the opened part as display partSetDisplayPartOnlyWhenOpen Set the opened part as display part only when it doesn’t exist in the sessionAlwaysSetDisplayPart Always set the opened part as display part whether it exists in the session-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-