SectionCollection Class¶
-
class
NXOpen.
SectionCollection
¶ Bases:
object
This class contains the factory methods for creating a section.
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
CreateSection | Creates a section. |
CreateSectionsUsingCurves | Creates sections using curves such that each section can be extruded to produce one body. |
Enumerations¶
SectionCollectionLoopOption Enumeration | Defines how section are created in SectionCollection.CreateSectionsUsingCurves |
Method Detail¶
CreateSection¶
-
SectionCollection.
CreateSection
¶ Overloaded method CreateSection
CreateSection(chainingTolerance, distanceTolerance, angleTolerance)
CreateSection()
CreateSection(curve)
-------------------------------------
Creates a section.
You should add selection intent rules to the section.
See the documentation for
Section.AddToSection
for more details.You can remove selection intent rules or one section element from the section.
See the documentation for
Section.RemoveRules
andSection.RemoveSingleSectionElement
for more details.Signature
CreateSection(chainingTolerance, distanceTolerance, angleTolerance)
Parameters: - chainingTolerance (float) – Chaining tolerance
- distanceTolerance (float) – Distance tolerance
- angleTolerance (float) – Angle tolerance
Returns: Return type: New in version NX3.0.0.
License requirements: gateway (“UG GATEWAY”)
-------------------------------------
Creates a section using default values for chaining, distance, and angle tolerance.
You should add selection intent rules to the section.
See the documentation for
Section.AddToSection
for more details.You can remove selection intent rules or one section element from the section.
See the documentation for
Section.RemoveRules
andSection.RemoveSingleSectionElement
for more details.Signature
CreateSection()
Returns: Return type: NXOpen.Section
New in version NX3.0.0.
License requirements: gateway (“UG GATEWAY”)
-------------------------------------
Creates a section with Single Curve rule using the given curve, edge or point.
Signature
CreateSection(curve)
Parameters: curve ( NXOpen.NXObject
) – Curve, Edge or PointReturns: The created section Return type: NXOpen.Section
New in version NX8.0.0.
License requirements: gateway (“UG GATEWAY”)
-------------------------------------
CreateSectionsUsingCurves¶
-
SectionCollection.
CreateSectionsUsingCurves
¶ Creates sections using curves such that each section can be extruded to produce one body.
Curves are first sorted into loops and then the loops are classified as exterior loops and interior loops. A section is created for each exterior loop of curves and includes closed loops that are enclosed in the exterior loop depending on the loop option.
The inputs must be all curves. The curves must lie on the same plane.
Signature
CreateSectionsUsingCurves(curves, loopOption, chainingTolerance, distanceTolerance, angleTolerance)
Parameters: - curves (list of
NXOpen.NXObject
) – Curves - loopOption (
NXOpen.SectionCollectionLoopOption
) – Loop option - chainingTolerance (float) – Chaining tolerance
- distanceTolerance (float) – Distance tolerance
- angleTolerance (float) – Angle tolerance
Returns: Return type: list of
NXOpen.Section
New in version NX4.0.4.
License requirements: gateway (“UG GATEWAY”)
- curves (list of