KinematicComponentBuilderSystemClass Enumeration¶
NXOpen.SIM.KinematicComponentBuilder.SystemClass is an alias for NXOpen.SIM.KinematicComponentBuilderSystemClass
-
class
NXOpen.SIM.
KinematicComponentBuilderSystemClass
¶ Bases:
object
The SIM KIM system classes
Enum Members
If this bit is set, then the machine part can be used for simulation when only UG_ISV_BASIC license is available “
“LatheSpindle”, ” lathe spindle class ” “PocketOnHead”, ” Pocket on a machine head class ” “ToolCutting”, ” Cutting portion of a tool ” “Spinning”, ” Component defines spinning geometry ” “Head”, ” Head class “-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-