RuleManagerDebugInstance_Struct Struct¶
NXOpen.RuleManager.DebugInstance is an alias for NXOpen.RuleManagerDebugInstance_Struct
-
class
NXOpen.
RuleManagerDebugInstance_Struct
¶ Bases:
object
Used to return debug update information for instances.
Fields¶
Field | Description |
---|---|
PartName | part of instance |
RefChain | name of instance |
NhaChain | nha of instance |
NRules | number of rules |
Rules0 | index of rules[0] |
PartName¶
-
RuleManagerDebugInstance_Struct.
PartName
¶ part of instance
-------------------------------------
Getter Method Signature
PartName()
Returns: Return type: str -------------------------------------
Setter Method
Signature
PartName(value)
Parameters: value (str) –
RefChain¶
-
RuleManagerDebugInstance_Struct.
RefChain
¶ name of instance
-------------------------------------
Getter Method Signature
RefChain()
Returns: Return type: str -------------------------------------
Setter Method
Signature
RefChain(value)
Parameters: value (str) –
NhaChain¶
-
RuleManagerDebugInstance_Struct.
NhaChain
¶ nha of instance
-------------------------------------
Getter Method Signature
NhaChain()
Returns: Return type: str -------------------------------------
Setter Method
Signature
NhaChain(value)
Parameters: value (str) –