SystemDeviceCollection Class¶
-
class
NXOpen.Routing.Electrical.
SystemDeviceCollection
¶ Bases:
object
Represents a collection of
NXOpen.Routing.Electrical.SystemDevice
objects.To obtain an instance of this class, refer to
NXOpen.Routing.RouteManager
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreateSystemDevice | Creates NXOpen.Routing.Electrical.SystemDevice . |
GetSystemSingleDevices | Get System Devices. |
Method Detail¶
CreateSystemDevice¶
-
SystemDeviceCollection.
CreateSystemDevice
¶ Overloaded method CreateSystemDevice
CreateSystemDevice()
CreateSystemDevice(systemName)
-------------------------------------
Creates
NXOpen.Routing.Electrical.SystemDevice
.Signature
CreateSystemDevice()
Returns: The new System Device. Return type: NXOpen.Routing.Electrical.SystemDevice
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Creates
NXOpen.Routing.Electrical.SystemDevice
with given name.Signature
CreateSystemDevice(systemName)
Parameters: systemName (str) – The name of the new system. (None not allowed) NOTE: The full Unicode character set is not supported for this parameter. Returns: The new System Device. Return type: NXOpen.Routing.Electrical.SystemDevice
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
GetSystemSingleDevices¶
-
SystemDeviceCollection.
GetSystemSingleDevices
¶ Get System Devices.
Signature
GetSystemSingleDevices()
Returns: The array of System Devices in the given part. Return type: list of NXOpen.Routing.Electrical.SystemDevice
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)