HarnessDeviceCollection Class¶
-
class
NXOpen.Routing.Electrical.
HarnessDeviceCollection
¶ Bases:
object
Represents a collection of
Routing.Electrical.HarnessDevice
objects.To obtain an instance of this class, refer to
NXOpen.Routing.RouteManager
New in version NX4.0.2.
Methods¶
Method | Description |
---|---|
CreateHarnessDevice | Creates Routing.Electrical.HarnessDevice . |
GetHarnessSingleDevices | Get harnesses @return |
Method Detail¶
CreateHarnessDevice¶
-
HarnessDeviceCollection.
CreateHarnessDevice
¶ Overloaded method CreateHarnessDevice
CreateHarnessDevice()
CreateHarnessDevice(harnessName)
-------------------------------------
Creates
Routing.Electrical.HarnessDevice
.Signature
CreateHarnessDevice()
Returns: Return type: NXOpen.Routing.Electrical.HarnessDevice
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Creates
Routing.Electrical.HarnessDevice
with given name.Signature
CreateHarnessDevice(harnessName)
Parameters: harnessName (str) – NOTE: The full Unicode character set is not supported for this parameter. Returns: Return type: NXOpen.Routing.Electrical.HarnessDevice
New in version NX5.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
GetHarnessSingleDevices¶
-
HarnessDeviceCollection.
GetHarnessSingleDevices
¶ Get harnesses
Signature
GetHarnessSingleDevices()
Returns: Return type: list of NXOpen.Routing.Electrical.HarnessDevice
New in version NX4.0.2.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)