RemoteUtilities Class¶
-
class
NXOpen.
RemoteUtilities
¶ Bases:
NXOpen.TaggedObject
This class is primarily designed for use in a remote session, and allows client applications to access resources on a remote server.
Note that due to security considerations, this class is independent of the main
NXOpen.Session
. The server must explicitly export a RemoteUtilities object in order to allow clients to access the methods in this class. Application writers should be aware that this class will allow clients to delete and modify files on the server.To obtain an instance of this class use
RemoteUtilities.GetRemoteUtilities
New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
CopyFile | Copies a file. |
CreateDirectory | Creates a directory. |
DeleteFile | Deletes a file. |
FileExists | Tests to see that a file exists @return True if the file exists |
GetEnvironmentVariable | Gets the value of an environment variable. |
IsFileWritable | Returns true if a file exists, and is writable by the NX session. |
RemoveDirectory | Deletes a directory. |
RenameFile | Renames a file. |
SetFileWritable | Sets a file’s permissions to be writable by the NX session. |
Method Detail¶
CopyFile¶
-
RemoteUtilities.
CopyFile
¶ Copies a file.
Signature
CopyFile(originalFilename, newFilename)
Parameters: - originalFilename (str) – Original filename. NOTE: The full Unicode character set is not supported for this parameter.
- newFilename (str) – Newly copied filename. NOTE: The full Unicode character set is not supported for this parameter.
New in version NX3.0.0.
License requirements: None.
CreateDirectory¶
-
RemoteUtilities.
CreateDirectory
¶ Creates a directory.
Signature
CreateDirectory(dirname)
Parameters: dirname (str) – Name of new directory NOTE: The full Unicode character set is not supported for this parameter. New in version NX3.0.0.
License requirements: None.
DeleteFile¶
-
RemoteUtilities.
DeleteFile
¶ Deletes a file.
Note that if the file does not exist, this method returns without any errors.
Signature
DeleteFile(filename)
Parameters: filename (str) – File to be deleted. NOTE: The full Unicode character set is not supported for this parameter. New in version NX3.0.0.
License requirements: None.
FileExists¶
-
RemoteUtilities.
FileExists
¶ Tests to see that a file exists
Signature
FileExists(testFilename)
Parameters: testFilename (str) – Filename to query NOTE: The full Unicode character set is not supported for this parameter. Returns: True if the file exists Return type: bool New in version NX3.0.0.
License requirements: None.
GetEnvironmentVariable¶
-
RemoteUtilities.
GetEnvironmentVariable
¶ Gets the value of an environment variable.
Signature
GetEnvironmentVariable(variableName)
Parameters: variableName (str) – The environment variable NOTE: The full Unicode character set is not supported for this parameter. Returns: The value of the variable. Return type: str New in version NX3.0.0.
Deprecated since version NX8.0.0: Use Session.GetEnvironmentVariable instead.
License requirements: None.
IsFileWritable¶
-
RemoteUtilities.
IsFileWritable
¶ Returns true if a file exists, and is writable by the NX session.
Signature
IsFileWritable(filename)
Parameters: filename (str) – File to be checked. NOTE: The full Unicode character set is not supported for this parameter. Returns: True if the file exists, and is writable Return type: bool New in version NX3.0.0.
License requirements: None.
RemoveDirectory¶
-
RemoteUtilities.
RemoveDirectory
¶ Deletes a directory.
Signature
RemoveDirectory(dirname)
Parameters: dirname (str) – Name of directory to be deleted NOTE: The full Unicode character set is not supported for this parameter. New in version NX3.0.0.
License requirements: None.
RenameFile¶
-
RemoteUtilities.
RenameFile
¶ Renames a file.
Signature
RenameFile(oldFilename, newFilename)
Parameters: - oldFilename (str) – Old filename. NOTE: The full Unicode character set is not supported for this parameter.
- newFilename (str) – New filename. NOTE: The full Unicode character set is not supported for this parameter.
New in version NX3.0.0.
License requirements: None.
SetFileWritable¶
-
RemoteUtilities.
SetFileWritable
¶ Sets a file’s permissions to be writable by the NX session.
Signature
SetFileWritable(filename, writable)
Parameters: - filename (str) – File to be checked. NOTE: The full Unicode character set is not supported for this parameter.
- writable (bool) – True to make the file writable, false to make it readonly
New in version NX3.0.0.
License requirements: None.