PrintPDFBuilder Class¶
-
class
NXOpen.
PrintPDFBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.PrintPDFBuilder
to be used when exporting the Current Display or selected sheets to a PDF document.This class is for use on Windows only and is created using
NXOpen.PlotManager
.To create a new instance of this class, use
NXOpen.PlotManager.CreatePrintPdfbuilder
Default values.
Property Value Relation Undefined New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Action | Returns or sets the action option to be used when saving the PDF file in a Teamcenter environment. |
AddWatermark | Returns or sets the Add Watermark option. |
Append | Returns or sets the Append option. |
Colors | Returns or sets the color option to be used when creating the PDF document. |
DatasetName | Returns or sets the dataset name to be used when Creating a New PDF document in a Teamcenter environment. |
DatasetType | Returns or sets the dataset type to be used when exporting a PDF to Teamcenter |
Filename | Returns or sets the filename to be used upon creation of the PDF document. |
ImageResolution | Returns or sets the resolution of images created for export of shaded views. |
NamedReferenceType | Returns or sets the named reference type to be used when exporting a PDF to Teamcenter |
OutputText | Returns or sets the output text of the PDF. |
RasterImages | Returns or sets the Raster Images option. |
Relation | Returns or sets the relation to be used when exporting a PDF to Teamcenter |
Scale | Returns or sets the scale factor to be used when creating a PDF document. |
ShadedGeometry | Returns or sets the Shaded Geometry as Wireframe option. |
Size | Returns or sets the size of the PDF document. |
SourceBuilder | Returns the Source builder. |
Tag | Returns the Tag for this object. |
Units | Returns or sets the units of the X and Y dimensions to be used when Dimension has been selected from the Size option. |
Watermark | Returns or sets the watermark text. |
Widths | Returns or sets the width option. |
XDimension | Returns or sets the x dimension to be used when Dimension has been selected from the Size option. |
YDimension | Returns or sets the y dimension to be used when Dimension has been selected from the Size option. |
Methods¶
Method | Description |
---|---|
Assign | The Assign button will assign an appropriate name to the Dataset field if Create New is chosen as the Action. |
Commit | Commits any edits that have been applied to the builder. |
CreateCdf | Creates and returns a NXOpen.CDF object representing the Color Palette. |
CreateWidthDefinition | Creates and returns a NXOpen.WidthDefinition object representing the Width Palette. |
DefinePalette | Initialize the Color Palette. |
DefineWidths | Initialize the Width dialog. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCdf | Returns a NXOpen.CDF object representing the Color Palette. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetWidthDefinition | Returns a NXOpen.WidthDefinition object representing the Width Palette. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PrintPDFBuilderActionOption Enumeration | Specifies the action option to be used when running Teamcenter |
PrintPDFBuilderColor Enumeration | Specifies the color option to use when creating the PDF document |
PrintPDFBuilderImageResolutionOption Enumeration | Specifies the image resolution when exporting a raster image |
PrintPDFBuilderOutputTextOption Enumeration | Specifies the output text option, as either text or polylines |
PrintPDFBuilderRelationOption Enumeration | Specifies the relation to use when exporting a PDF to Teamcenter |
PrintPDFBuilderSizeOption Enumeration | Specifies the size option of the PDF document. |
PrintPDFBuilderUnitsOption Enumeration | Specifies which units are associated to the dimensions |
PrintPDFBuilderWidth Enumeration | Specifies the primary selection of which type of width assignment to use. |
Property Detail¶
Action¶
-
PrintPDFBuilder.
Action
¶ Returns or sets the action option to be used when saving the PDF file in a Teamcenter environment.
This can be set to Create New, Overwrite Existing PDF, or Append to Existing PDF.
-------------------------------------
Getter Method
Signature
Action()
Returns: Return type: NXOpen.PrintPDFBuilderActionOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Action(action)
Parameters: action ( NXOpen.PrintPDFBuilderActionOption
) –New in version NX5.0.0.
License requirements: None.
AddWatermark¶
-
PrintPDFBuilder.
AddWatermark
¶ Returns or sets the Add Watermark option.
If Add Watermark is set to false, no Watermark will be added to the PDF document. If Add Watermark is set to true, the user defined watermark text will be added as a watermark to the PDF document.
-------------------------------------
Getter Method
Signature
AddWatermark()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AddWatermark(addWatermark)
Parameters: addWatermark (bool) – New in version NX5.0.0.
License requirements: None.
Append¶
-
PrintPDFBuilder.
Append
¶ Returns or sets the Append option.
If Append is set to false, a new PDF document will be created and will overwrite an existing PDF document. If Append is set to true, the selected sheets will be appended to the existing PDF document.
-------------------------------------
Getter Method
Signature
Append()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Append(append)
Parameters: append (bool) – New in version NX5.0.0.
License requirements: None.
Colors¶
-
PrintPDFBuilder.
Colors
¶ Returns or sets the color option to be used when creating the PDF document.
If the color option is set to Custom Palette or Colors By Width then the PDF document will be created with the user defined color attributes belonging to the CDF object.
-------------------------------------
Getter Method
Signature
Colors()
Returns: Return type: NXOpen.PrintPDFBuilderColor
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Colors(colors)
Parameters: colors ( NXOpen.PrintPDFBuilderColor
) –New in version NX5.0.0.
License requirements: None.
DatasetName¶
-
PrintPDFBuilder.
DatasetName
¶ Returns or sets the dataset name to be used when Creating a New PDF document in a Teamcenter environment.
The dataset name will be used if Create New, Overwrite Existing PDF, or Append to Existing PDF are selected as the Action.
-------------------------------------
Getter Method
Signature
DatasetName()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DatasetName(datasetName)
Parameters: datasetName (str) – New in version NX5.0.0.
License requirements: None.
DatasetType¶
-
PrintPDFBuilder.
DatasetType
¶ Returns or sets the dataset type to be used when exporting a PDF to Teamcenter
-------------------------------------
Getter Method
Signature
DatasetType()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DatasetType(datasetType)
Parameters: datasetType (str) – New in version NX7.5.0.
License requirements: None.
Filename¶
-
PrintPDFBuilder.
Filename
¶ Returns or sets the filename to be used upon creation of the PDF document.
-------------------------------------
Getter Method
Signature
Filename()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Filename(filename)
Parameters: filename (str) – New in version NX5.0.0.
License requirements: None.
ImageResolution¶
-
PrintPDFBuilder.
ImageResolution
¶ Returns or sets the resolution of images created for export of shaded views.
-------------------------------------
Getter Method
Signature
ImageResolution()
Returns: Return type: NXOpen.PrintPDFBuilderImageResolutionOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImageResolution(imageResolution)
Parameters: imageResolution ( NXOpen.PrintPDFBuilderImageResolutionOption
) –New in version NX5.0.0.
License requirements: None.
NamedReferenceType¶
-
PrintPDFBuilder.
NamedReferenceType
¶ Returns or sets the named reference type to be used when exporting a PDF to Teamcenter
-------------------------------------
Getter Method
Signature
NamedReferenceType()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NamedReferenceType(namedReferenceType)
Parameters: namedReferenceType (str) – New in version NX7.5.0.
License requirements: None.
OutputText¶
-
PrintPDFBuilder.
OutputText
¶ Returns or sets the output text of the PDF.
This will determine whether the drawing text will be exported as text or as polylines.
-------------------------------------
Getter Method
Signature
OutputText()
Returns: Return type: NXOpen.PrintPDFBuilderOutputTextOption
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputText(outputText)
Parameters: outputText ( NXOpen.PrintPDFBuilderOutputTextOption
) –New in version NX6.0.0.
License requirements: None.
RasterImages¶
-
PrintPDFBuilder.
RasterImages
¶ Returns or sets the Raster Images option.
This option determines whether or not raster images will be exported to the PDF document.
-------------------------------------
Getter Method
Signature
RasterImages()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RasterImages(rasterImages)
Parameters: rasterImages (bool) – New in version NX5.0.0.
License requirements: None.
Relation¶
-
PrintPDFBuilder.
Relation
¶ Returns or sets the relation to be used when exporting a PDF to Teamcenter
-------------------------------------
Getter Method
Signature
Relation()
Returns: Return type: NXOpen.PrintPDFBuilderRelationOption
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Relation(relation)
Parameters: relation ( NXOpen.PrintPDFBuilderRelationOption
) –New in version NX7.5.0.
License requirements: None.
Scale¶
-
PrintPDFBuilder.
Scale
¶ Returns or sets the scale factor to be used when creating a PDF document.
This value ranges from 0.00 to 1.00 and will only be used if the Size option is set to Scale.
-------------------------------------
Getter Method
Signature
Scale()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Scale(scale)
Parameters: scale (float) – New in version NX5.0.0.
License requirements: None.
ShadedGeometry¶
-
PrintPDFBuilder.
ShadedGeometry
¶ Returns or sets the Shaded Geometry as Wireframe option.
If set to true, this option will show shaded objects as wireframes. The shaded objects will be represented as shaded if this option is set to false.
-------------------------------------
Getter Method
Signature
ShadedGeometry()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShadedGeometry(shadedGeometry)
Parameters: shadedGeometry (bool) – New in version NX5.0.0.
License requirements: None.
Size¶
-
PrintPDFBuilder.
Size
¶ Returns or sets the size of the PDF document.
If the size is set to Scale, then the PDF will use the user-defined Scale Factor. If the size is set to dimension, then the PDF will use the user-defined X and Y dimensions.
-------------------------------------
Getter Method
Signature
Size()
Returns: Return type: NXOpen.PrintPDFBuilderSizeOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Size(size)
Parameters: size ( NXOpen.PrintPDFBuilderSizeOption
) –New in version NX5.0.0.
License requirements: None.
SourceBuilder¶
-
PrintPDFBuilder.
SourceBuilder
¶ Returns the Source builder.
The Source builder contains all data involving the selected sheets.
-------------------------------------
Getter Method
Signature
SourceBuilder()
Returns: New SourceBuilder object Return type: NXOpen.PlotSourceBuilder
New in version NX5.0.1.
License requirements: None.
Units¶
-
PrintPDFBuilder.
Units
¶ Returns or sets the units of the X and Y dimensions to be used when Dimension has been selected from the Size option.
-------------------------------------
Getter Method
Signature
Units()
Returns: Return type: NXOpen.PrintPDFBuilderUnitsOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Units(units)
Parameters: units ( NXOpen.PrintPDFBuilderUnitsOption
) –New in version NX5.0.0.
License requirements: None.
Watermark¶
-
PrintPDFBuilder.
Watermark
¶ Returns or sets the watermark text.
This user-defined text will appear as a watermark to the PDF document only if Add Watermark is set to true.
-------------------------------------
Getter Method
Signature
Watermark()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Watermark(watermark)
Parameters: watermark (str) – New in version NX5.0.0.
License requirements: None.
Widths¶
-
PrintPDFBuilder.
Widths
¶ Returns or sets the width option.
If the width option is set to Single Width, Custom Three Widths, or Custom Palette then the PDF document will be created with the user defined width attributes belonging to the WidthDefinition object.
-------------------------------------
Getter Method
Signature
Widths()
Returns: Return type: NXOpen.PrintPDFBuilderWidth
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Widths(widths)
Parameters: widths ( NXOpen.PrintPDFBuilderWidth
) –New in version NX5.0.0.
License requirements: None.
XDimension¶
-
PrintPDFBuilder.
XDimension
¶ Returns or sets the x dimension to be used when Dimension has been selected from the Size option.
-------------------------------------
Getter Method
Signature
XDimension()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
XDimension(xDimension)
Parameters: xDimension (float) – New in version NX5.0.0.
License requirements: None.
YDimension¶
-
PrintPDFBuilder.
YDimension
¶ Returns or sets the y dimension to be used when Dimension has been selected from the Size option.
-------------------------------------
Getter Method
Signature
YDimension()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
YDimension(yDimension)
Parameters: yDimension (float) – New in version NX5.0.0.
License requirements: None.
Method Detail¶
Assign¶
-
PrintPDFBuilder.
Assign
¶ The Assign button will assign an appropriate name to the Dataset field if Create New is chosen as the Action.
Signature
Assign()
New in version NX5.0.0.
License requirements: None.
CreateCdf¶
-
PrintPDFBuilder.
CreateCdf
¶ Creates and returns a
NXOpen.CDF
object representing the Color Palette.This object contains all custom color information to be used when Custom Palette or Colors By Width is selected from the Color option.
Signature
CreateCdf()
Returns: CDF object Return type: NXOpen.CDF
New in version NX5.0.0.
License requirements: None.
CreateWidthDefinition¶
-
PrintPDFBuilder.
CreateWidthDefinition
¶ Creates and returns a
NXOpen.WidthDefinition
object representing the Width Palette.This object contains all custom width information to be used when Single Width, Custom Three Widths, or Custom Palette is selected from the Width option.
Signature
CreateWidthDefinition()
Returns: WidthDefinition object Return type: NXOpen.WidthDefinition
New in version NX5.0.0.
License requirements: None.
DefinePalette¶
-
PrintPDFBuilder.
DefinePalette
¶ Initialize the Color Palette.
This allows the user to change the attributes of any color. These changed colors will be used if Custom Palette or Colors By Width is selected as the color option.
Signature
DefinePalette()
New in version NX5.0.0.
License requirements: None.
DefineWidths¶
-
PrintPDFBuilder.
DefineWidths
¶ Initialize the Width dialog.
This allows the user to change the attributes of Single Width, Custom Three Widths, or Custom Palette. These changed width values will be used depending on the width option selected.
Signature
DefineWidths()
New in version NX5.0.0.
License requirements: None.
GetCdf¶
-
PrintPDFBuilder.
GetCdf
¶ Returns a
NXOpen.CDF
object representing the Color Palette.This object contains all custom color information to be used when Custom Palette or Colors By Width is selected from the Color option.
Signature
GetCdf()
Returns: CDF object Return type: NXOpen.CDF
New in version NX5.0.0.
License requirements: None.
GetWidthDefinition¶
-
PrintPDFBuilder.
GetWidthDefinition
¶ Returns a
NXOpen.WidthDefinition
object representing the Width Palette.This object contains all custom width information to be used when Single Width, Custom Three Widths, or Custom Palette is selected from the Width option.
Signature
GetWidthDefinition()
Returns: WidthDefinition object Return type: NXOpen.WidthDefinition
New in version NX5.0.0.
License requirements: None.
Validate¶
-
PrintPDFBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.