PrintBuilder Class¶
-
class
NXOpen.
PrintBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.PrintBuilder
.This class is for use on Windows only and contains all information relating to printing. It is created using
NXOpen.PlotManager
.The user must specify the sheets to be printed by setting the appropriate fields through the
NXOpen.PlotSourceBuilder
. The printer text and copies fields must be set in order to successfully print the provided sheets. The printer text is the path of the desired printer and the copies field represents the number of copies to be printed. This class also allows for the line widths to be scaled by setting the appropriate thin, normal, or thick scale factors.To create a new instance of this class, use
NXOpen.PlotManager.CreatePrintBuilder
Default values.
Property Value Orientation Landscape Width1ScaleFactor 1.0 Width2ScaleFactor 2.0 Width3ScaleFactor 3.0 Width4ScaleFactor 4.0 Width5ScaleFactor 5.0 Width6ScaleFactor 6.0 Width7ScaleFactor 7.0 Width8ScaleFactor 8.0 Width9ScaleFactor 9.0 New in version NX5.0.1.
Properties¶
Property | Description |
---|---|
Copies | Returns or sets the number of copies. |
CustomPaper | Returns or sets the custom paper. |
ImageResolution | Returns or sets the resolution of images created for printing shaded views. |
NormalWidth | Returns or sets the normal width scale factor. |
Orientation | Returns or sets the orientation. |
Output | Returns or sets the shaded image option. |
Paper | Returns or sets the paper. |
PrinterText | Returns or sets the printer text. |
RasterImages | Returns or sets the raster images option. |
ShadedGeometry | Returns or sets the shaded geometry as wireframe option. |
SourceBuilder | Returns the Source builder. |
Tag | Returns the Tag for this object. |
ThickWidth | Returns or sets the thick width scale factor. |
ThinWidth | Returns or sets the thin width scale factor. |
WhiteBackground | Returns or sets the white background option. |
Width1ScaleFactor | Returns or sets the width1 scale factor. |
Width2ScaleFactor | Returns or sets the width2 scale factor. |
Width3ScaleFactor | Returns or sets the width3 scale factor. |
Width4ScaleFactor | Returns or sets the width4 scale factor. |
Width5ScaleFactor | Returns or sets the width5 scale factor. |
Width6ScaleFactor | Returns or sets the width6 scale factor. |
Width7ScaleFactor | Returns or sets the width7 scale factor. |
Width8ScaleFactor | Returns or sets the width8 scale factor. |
Width9ScaleFactor | Returns or sets the width9 scale factor. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PrintBuilderImageResolutionOption Enumeration | Specifies the print image resolution |
PrintBuilderOrientationOption Enumeration | Specifies the orientation of the printed sheet |
PrintBuilderOutputOption Enumeration | Specifies the output option when printing Current Display |
PrintBuilderPaperSize Enumeration | Specifies the paper size of the printed sheet |
Property Detail¶
Copies¶
-
PrintBuilder.
Copies
¶ Returns or sets the number of copies.
This option specifies the number of copies to be printed.
-------------------------------------
Getter Method
Signature
Copies()
Returns: Return type: int New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
Copies(copies)
Parameters: copies (int) – New in version NX5.0.1.
License requirements: None.
CustomPaper¶
-
PrintBuilder.
CustomPaper
¶ Returns or sets the custom paper.
This will be used if the paper size is set to Custom.
-------------------------------------
Getter Method
Signature
CustomPaper()
Returns: Return type: int New in version NX6.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
CustomPaper(customPaper)
Parameters: customPaper (int) – New in version NX6.0.2.
License requirements: None.
ImageResolution¶
-
PrintBuilder.
ImageResolution
¶ Returns or sets the resolution of images created for printing shaded views.
-------------------------------------
Getter Method
Signature
ImageResolution()
Returns: Return type: NXOpen.PrintBuilderImageResolutionOption
New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImageResolution(imageResolution)
Parameters: imageResolution ( NXOpen.PrintBuilderImageResolutionOption
) –New in version NX5.0.1.
License requirements: None.
NormalWidth¶
-
PrintBuilder.
NormalWidth
¶ Returns or sets the normal width scale factor.
This number is used as a scale factor for normal width lines. It cannot be less than 0.0.
-------------------------------------
Getter Method
Signature
NormalWidth()
Returns: Return type: float New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
NormalWidth(normalWidth)
Parameters: normalWidth (float) – New in version NX5.0.1.
License requirements: None.
Orientation¶
-
PrintBuilder.
Orientation
¶ Returns or sets the orientation.
This options determines the orientation of the printed page.
-------------------------------------
Getter Method
Signature
Orientation()
Returns: Return type: NXOpen.PrintBuilderOrientationOption
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Orientation(orientationOption)
Parameters: orientationOption ( NXOpen.PrintBuilderOrientationOption
) –New in version NX6.0.0.
License requirements: None.
Output¶
-
PrintBuilder.
Output
¶ Returns or sets the shaded image option.
The Current Display will be printed using the correct current shading if this option is set.
-------------------------------------
Getter Method
Signature
Output()
Returns: Return type: NXOpen.PrintBuilderOutputOption
New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
Output(outputOption)
Parameters: outputOption ( NXOpen.PrintBuilderOutputOption
) –New in version NX5.0.1.
License requirements: None.
Paper¶
-
PrintBuilder.
Paper
¶ Returns or sets the paper.
This options determines the paper size used for printing. Note that all options may not available on all printers.
-------------------------------------
Getter Method
Signature
Paper()
Returns: Return type: NXOpen.PrintBuilderPaperSize
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Paper(paper)
Parameters: paper ( NXOpen.PrintBuilderPaperSize
) –New in version NX6.0.0.
License requirements: None.
PrinterText¶
-
PrintBuilder.
PrinterText
¶ Returns or sets the printer text.
The printer field represents the full path name of the printer the user wishes to print to.
-------------------------------------
Getter Method
Signature
PrinterText()
Returns: Return type: str New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
PrinterText(printer)
Parameters: printer (str) – New in version NX5.0.1.
License requirements: None.
RasterImages¶
-
PrintBuilder.
RasterImages
¶ Returns or sets the raster images option.
This option determines whether or not raster images will be used when printing.
-------------------------------------
Getter Method
Signature
RasterImages()
Returns: Return type: bool New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
RasterImages(rasterImages)
Parameters: rasterImages (bool) – New in version NX5.0.1.
License requirements: None.
ShadedGeometry¶
-
PrintBuilder.
ShadedGeometry
¶ Returns or sets the shaded geometry as wireframe option.
If set to true, this option will show shaded objects as wireframes. The shaded objects will be represented as shaded if this option is set to false.
-------------------------------------
Getter Method
Signature
ShadedGeometry()
Returns: Return type: bool New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShadedGeometry(shadedGeometry)
Parameters: shadedGeometry (bool) – New in version NX5.0.1.
License requirements: None.
SourceBuilder¶
-
PrintBuilder.
SourceBuilder
¶ Returns the Source builder.
The Source builder contains all data involving the sheets to to be printed.
-------------------------------------
Getter Method
Signature
SourceBuilder()
Returns: New SourceBuilder object Return type: NXOpen.PlotSourceBuilder
New in version NX5.0.1.
License requirements: None.
ThickWidth¶
-
PrintBuilder.
ThickWidth
¶ Returns or sets the thick width scale factor.
This number is used as a scale factor for thick width lines. It cannot be less than 0.0.
-------------------------------------
Getter Method
Signature
ThickWidth()
Returns: Return type: float New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThickWidth(thickWidth)
Parameters: thickWidth (float) – New in version NX5.0.1.
License requirements: None.
ThinWidth¶
-
PrintBuilder.
ThinWidth
¶ Returns or sets the thin width scale factor.
This number is used as a scale factor for thin width lines. It cannot be less than 0.0.
-------------------------------------
Getter Method
Signature
ThinWidth()
Returns: Return type: float New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThinWidth(thinWidth)
Parameters: thinWidth (float) – New in version NX5.0.1.
License requirements: None.
WhiteBackground¶
-
PrintBuilder.
WhiteBackground
¶ Returns or sets the white background option.
When printing a shaded view, this option allows for the background to be white. Only set to true if printing Current Display and “Shaded Image” is also set to true.
-------------------------------------
Getter Method
Signature
WhiteBackground()
Returns: Return type: bool New in version NX5.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
WhiteBackground(whiteBackground)
Parameters: whiteBackground (bool) – New in version NX5.0.1.
License requirements: None.
Width1ScaleFactor¶
-
PrintBuilder.
Width1ScaleFactor
¶ Returns or sets the width1 scale factor.
This number is used as a scale factor for width1 lines. It cannot be less than 0.0.
-------------------------------------
Getter Method
Signature
Width1ScaleFactor()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width1ScaleFactor(width1ScaleFactor)
Parameters: width1ScaleFactor (float) – New in version NX8.5.0.
License requirements: None.
Width2ScaleFactor¶
-
PrintBuilder.
Width2ScaleFactor
¶ Returns or sets the width2 scale factor.
This number is used as a scale factor for width2 lines. It cannot be less than 0.0.
-------------------------------------
Getter Method
Signature
Width2ScaleFactor()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width2ScaleFactor(width2ScaleFactor)
Parameters: width2ScaleFactor (float) – New in version NX8.5.0.
License requirements: None.
Width3ScaleFactor¶
-
PrintBuilder.
Width3ScaleFactor
¶ Returns or sets the width3 scale factor.
This number is used as a scale factor for width3 lines. It cannot be less than 0.0.
-------------------------------------
Getter Method
Signature
Width3ScaleFactor()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width3ScaleFactor(width3ScaleFactor)
Parameters: width3ScaleFactor (float) – New in version NX8.5.0.
License requirements: None.
Width4ScaleFactor¶
-
PrintBuilder.
Width4ScaleFactor
¶ Returns or sets the width4 scale factor.
This number is used as a scale factor for width4 lines. It cannot be less than 0.0.
-------------------------------------
Getter Method
Signature
Width4ScaleFactor()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width4ScaleFactor(width4ScaleFactor)
Parameters: width4ScaleFactor (float) – New in version NX8.5.0.
License requirements: None.
Width5ScaleFactor¶
-
PrintBuilder.
Width5ScaleFactor
¶ Returns or sets the width5 scale factor.
This number is used as a scale factor for width5 lines. It cannot be less than 0.0.
-------------------------------------
Getter Method
Signature
Width5ScaleFactor()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width5ScaleFactor(width5ScaleFactor)
Parameters: width5ScaleFactor (float) – New in version NX8.5.0.
License requirements: None.
Width6ScaleFactor¶
-
PrintBuilder.
Width6ScaleFactor
¶ Returns or sets the width6 scale factor.
This number is used as a scale factor for width6 lines. It cannot be less than 0.0.
-------------------------------------
Getter Method
Signature
Width6ScaleFactor()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width6ScaleFactor(width6ScaleFactor)
Parameters: width6ScaleFactor (float) – New in version NX8.5.0.
License requirements: None.
Width7ScaleFactor¶
-
PrintBuilder.
Width7ScaleFactor
¶ Returns or sets the width7 scale factor.
This number is used as a scale factor for width7 lines. It cannot be less than 0.0.
-------------------------------------
Getter Method
Signature
Width7ScaleFactor()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width7ScaleFactor(width7ScaleFactor)
Parameters: width7ScaleFactor (float) – New in version NX8.5.0.
License requirements: None.
Width8ScaleFactor¶
-
PrintBuilder.
Width8ScaleFactor
¶ Returns or sets the width8 scale factor.
This number is used as a scale factor for width8 lines. It cannot be less than 0.0.
-------------------------------------
Getter Method
Signature
Width8ScaleFactor()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width8ScaleFactor(width8ScaleFactor)
Parameters: width8ScaleFactor (float) – New in version NX8.5.0.
License requirements: None.
Width9ScaleFactor¶
-
PrintBuilder.
Width9ScaleFactor
¶ Returns or sets the width9 scale factor.
This number is used as a scale factor for width9 lines. It cannot be less than 0.0.
-------------------------------------
Getter Method
Signature
Width9ScaleFactor()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width9ScaleFactor(width9ScaleFactor)
Parameters: width9ScaleFactor (float) – New in version NX8.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
PrintBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.