WorkPlaneGridSize_Struct Struct¶
NXOpen.Preferences.WorkPlane.GridSize is an alias for NXOpen.Preferences.WorkPlaneGridSize_Struct
-
class
NXOpen.Preferences.
WorkPlaneGridSize_Struct
¶ Bases:
object
Grid size parameters
Fields¶
Field | Description |
---|---|
MajorGridSpacing | Distance between major grid lines |
MinorLinesPerMajor | Number of minor lines between major grid lines |
SnapPointsPerMinor | Number of snap points between minor grid lines |
MajorGridSpacing¶
-
WorkPlaneGridSize_Struct.
MajorGridSpacing
¶ Distance between major grid lines
-------------------------------------
Getter Method Signature
MajorGridSpacing()
Returns: Return type: float -------------------------------------
Setter Method
Signature
MajorGridSpacing(value)
Parameters: value (float) –
MinorLinesPerMajor¶
-
WorkPlaneGridSize_Struct.
MinorLinesPerMajor
¶ Number of minor lines between major grid lines
-------------------------------------
Getter Method Signature
MinorLinesPerMajor()
Returns: Return type: int -------------------------------------
Setter Method
Signature
MinorLinesPerMajor(value)
Parameters: value (int) –
SnapPointsPerMinor¶
-
WorkPlaneGridSize_Struct.
SnapPointsPerMinor
¶ Number of snap points between minor grid lines
-------------------------------------
Getter Method Signature
SnapPointsPerMinor()
Returns: Return type: int -------------------------------------
Setter Method
Signature
SnapPointsPerMinor(value)
Parameters: value (int) –