WorkPlaneGrid Enumeration¶
NXOpen.Preferences.WorkPlane.Grid is an alias for NXOpen.Preferences.WorkPlaneGrid
-
class
NXOpen.Preferences.
WorkPlaneGrid
¶ Bases:
object
Describes whether the Grid type selected is Polar or Rectangular
Enum Members
Enum Member Enum Member Description Polar Polar GridRectangular Rectangular Grid-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-