VisualizationHandles Class¶
-
class
NXOpen.Preferences.
VisualizationHandles
¶ Bases:
object
Represents the set of visualization preferences under handles tab applicable to entire session
To obtain an instance of this class, refer to
NXOpen.Preferences.SessionPreferences
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
HandleSize | Returns or sets the default handle size |
ShowHandleHints | Returns or sets the show handle hints flag. |
Methods¶
Enumerations¶
VisualizationHandlesHandleSizeValue Enumeration | Specifies size values for the default handle size. |
Property Detail¶
HandleSize¶
-
VisualizationHandles.
HandleSize
¶ Returns or sets the default handle size
-------------------------------------
Getter Method
Signature
HandleSize()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HandleSize(handleSize)
Parameters: handleSize (int) – New in version NX7.5.0.
License requirements: None.
ShowHandleHints¶
-
VisualizationHandles.
ShowHandleHints
¶ Returns or sets the show handle hints flag.
If true displays handle hint when handle is preselected
-------------------------------------
Getter Method
Signature
ShowHandleHints()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowHandleHints(showHandleHints)
Parameters: showHandleHints (bool) – New in version NX7.5.0.
License requirements: None.