ViewVisualizationVisualSmoothEdgeWidth Enumeration¶
NXOpen.Preferences.ViewVisualizationVisual.SmoothEdgeWidth is an alias for NXOpen.Preferences.ViewVisualizationVisualSmoothEdgeWidth
-
class
NXOpen.Preferences.
ViewVisualizationVisualSmoothEdgeWidth
¶ Bases:
object
Describes all possible width selection for visible smooth edges
Enum Members
Enum Member Enum Member Description Original Thin Normal Thick One Two Three Four Five Six Seven Eight Nine -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-