ViewVisualizationSpecialEffectsFogType Enumeration¶
NXOpen.Preferences.ViewVisualizationSpecialEffects.FogType is an alias for NXOpen.Preferences.ViewVisualizationSpecialEffectsFogType
-
class
NXOpen.Preferences.
ViewVisualizationSpecialEffectsFogType
¶ Bases:
object
Describes whether the fog type is selected as linear or light or heavy.
Enum Members
Enum Member Enum Member Description Linear Linear FogLight Non linear Fog. Light fog produces a fog effect less pervasive than Heavy fogHeavy Non linear Fog-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-