ViewVisualizationSpecialEffectsColorHLS_Struct Struct¶
NXOpen.Preferences.ViewVisualizationSpecialEffects.ColorHLS is an alias for NXOpen.Preferences.ViewVisualizationSpecialEffectsColorHLS_Struct
-
class
NXOpen.Preferences.
ViewVisualizationSpecialEffectsColorHLS_Struct
¶ Bases:
object
Represents three constituents of a HLS color pattern
Fields¶
Field | Description |
---|---|
Hue | Hue in HSV pattern is the color type (such as red, blue, or yellow) Ranges from 0-360 |
Lightness | Lightness in HLS pattern Ranges from 0-255 |
Saturation | Saturation in HSV pattern is the vibrancy of the color Ranges from 0-255 |
Hue¶
-
ViewVisualizationSpecialEffectsColorHLS_Struct.
Hue
¶ Hue in HSV pattern is the color type (such as red, blue, or yellow) Ranges from 0-360
-------------------------------------
Getter Method Signature
Hue()
Returns: Return type: float -------------------------------------
Setter Method
Signature
Hue(value)
Parameters: value (float) –
Lightness¶
-
ViewVisualizationSpecialEffectsColorHLS_Struct.
Lightness
¶ Lightness in HLS pattern Ranges from 0-255
-------------------------------------
Getter Method Signature
Lightness()
Returns: Return type: float -------------------------------------
Setter Method
Signature
Lightness(value)
Parameters: value (float) –
Saturation¶
-
ViewVisualizationSpecialEffectsColorHLS_Struct.
Saturation
¶ Saturation in HSV pattern is the “vibrancy” of the color Ranges from 0-255
-------------------------------------
Getter Method Signature
Saturation()
Returns: Return type: float -------------------------------------
Setter Method
Signature
Saturation(value)
Parameters: value (float) –