ViewSection Class¶
-
class
NXOpen.Preferences.
ViewSection
¶ Bases:
NXOpen.Builder
Records / queries view section preferences.
To obtain a instance of this class use
Preferences.SessionPreferences.CreateViewSectionPreference
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
LoadExact | Returns or sets the load exact geometry on a save section curves operation view section preference. |
Tag | Returns the Tag for this object. |
TranslucentPlanes | Returns or sets the translucent plane setting view section preference. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetDefaults | Set current view section preferences to the default customer default values. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
LoadExact¶
-
ViewSection.
LoadExact
¶ Returns or sets the load exact geometry on a save section curves operation view section preference.
-------------------------------------
Getter Method
Signature
LoadExact()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LoadExact(loadExact)
Parameters: loadExact (bool) – New in version NX7.5.0.
License requirements: None.
TranslucentPlanes¶
-
ViewSection.
TranslucentPlanes
¶ Returns or sets the translucent plane setting view section preference.
-------------------------------------
Getter Method
Signature
TranslucentPlanes()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TranslucentPlanes(translucentPlanes)
Parameters: translucentPlanes (bool) – New in version NX7.5.0.
License requirements: None.
Method Detail¶
SetDefaults¶
-
ViewSection.
SetDefaults
¶ Set current view section preferences to the default customer default values.
Signature
SetDefaults()
New in version NX7.5.0.
License requirements: None.
Validate¶
-
ViewSection.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.