TraceLinesViewPreferences Class¶
-
class
NXOpen.Preferences.
TraceLinesViewPreferences
¶ Bases:
object
Represents set of Trace Lines View Preferences applicable to drafting views.
To obtain an instance of this class use
Preferences.ViewPreferences.TraceLines
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CreateGapsStatus | Returns or sets the status of create gaps |
GapSize | Returns or sets the gap size. |
HiddenColor | Returns or sets the hidden color. |
HiddenFont | Returns or sets the hidden font |
HiddenWidth | Returns or sets the hidden width |
VisibleColor | Returns or sets the visible color. |
VisibleFont | Returns or sets the visible font |
VisibleWidth | Returns or sets the visible width |
Methods¶
Property Detail¶
CreateGapsStatus¶
-
TraceLinesViewPreferences.
CreateGapsStatus
¶ Returns or sets the status of create gaps
-------------------------------------
Getter Method
Signature
CreateGapsStatus()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateGapsStatus(createGaps)
Parameters: createGaps (bool) – New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
GapSize¶
-
TraceLinesViewPreferences.
GapSize
¶ Returns or sets the gap size.
-------------------------------------
Getter Method
Signature
GapSize()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GapSize(gapSize)
Parameters: gapSize (float) – New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
VisibleColor¶
-
TraceLinesViewPreferences.
VisibleColor
¶ Returns or sets the visible color.
The value should be between 1 and 216.
-------------------------------------
Getter Method
Signature
VisibleColor()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisibleColor(visibleColor)
Parameters: visibleColor (int) – New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
VisibleFont¶
-
TraceLinesViewPreferences.
VisibleFont
¶ Returns or sets the visible font
-------------------------------------
Getter Method
Signature
VisibleFont()
Returns: Return type: NXOpen.Preferences.Font
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisibleFont(visibleFont)
Parameters: visibleFont ( NXOpen.Preferences.Font
) –New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)
VisibleWidth¶
-
TraceLinesViewPreferences.
VisibleWidth
¶ Returns or sets the visible width
-------------------------------------
Getter Method
Signature
VisibleWidth()
Returns: Return type: NXOpen.Preferences.Width
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VisibleWidth(visibleWidth)
Parameters: visibleWidth ( NXOpen.Preferences.Width
) –New in version NX5.0.0.
License requirements: drafting (“DRAFTING”)