SessionVisualizationVisual Class¶
Properties¶
Property | Description |
---|---|
FullSceneAntialiasing | Returns or sets the scene antialiasing flag. |
LineAntialiasing | Returns or sets the line antialiasing flag. |
Translucency | Returns or sets the translucency flag. |
Methods¶
Property Detail¶
FullSceneAntialiasing¶
-
SessionVisualizationVisual.
FullSceneAntialiasing
¶ Returns or sets the scene antialiasing flag.
-------------------------------------
Getter Method
Signature
FullSceneAntialiasing()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FullSceneAntialiasing(fullSceneAntialiasing)
Parameters: fullSceneAntialiasing (bool) – New in version NX3.0.0.
License requirements: None.
LineAntialiasing¶
-
SessionVisualizationVisual.
LineAntialiasing
¶ Returns or sets the line antialiasing flag.
True value specifies that lines, curves, and edges are drawn more smoothly
-------------------------------------
Getter Method
Signature
LineAntialiasing()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LineAntialiasing(lineAntialiasing)
Parameters: lineAntialiasing (bool) – New in version NX3.0.0.
License requirements: None.
Translucency¶
-
SessionVisualizationVisual.
Translucency
¶ Returns or sets the translucency flag.
True value specifies that each shaded object is drawn with the translucency setting specified with Edit-<ja_gt>Object Display. False value specify that all objects in Fully Shaded or Partially Shaded views appear opaque, regardless of their individual translucency settings.
-------------------------------------
Getter Method
Signature
Translucency()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Translucency(translucency)
Parameters: translucency (bool) – New in version NX3.0.0.
License requirements: None.