SessionVisualizationShadeSeeThruOptions_Struct Struct¶
NXOpen.Preferences.SessionVisualizationShade.SeeThruOptions is an alias for NXOpen.Preferences.SessionVisualizationShadeSeeThruOptions_Struct
-
class
NXOpen.Preferences.
SessionVisualizationShadeSeeThruOptions_Struct
¶ Bases:
object
Specifies the See-Thru color, edge, and translucency options used for the various See-Thru Styles.
Deprecated since version NX8.5.0: See
NXOpen.Preferences.PartVisualizationEmphasis
.
Fields¶
Field | Description |
---|---|
ShellRgb | Specifies the color of less important shaded geometry when See-Thru Style is set to Shell. |
ShellEdges | Determines whether edges are displayed for less important shaded geometry when See-Thru Style is set to Shell. |
ShellEdgesRgb | Specifies the color of edges displayed for less important shaded geometry when See-Thru Style is set to Shell. |
ShellTranslucency | Translucency percentage applied to less important shaded geometry when See-Thru Style is set to Shell. |
OriginalColorShellEdges | Determines whether edges are displayed for less important shaded geometry when See-Thru Style is set to Original Color Shell. |
OriginalColorShellEdgesRgb | Specifies the color of edges displayed for less important shaded geometry when See-Thru Style is set to Original Color Shell. |
OriginalColorShellTranslucency | Translucency percentage applied to less important shaded geometry when See-Thru Style is set to Original Color Shell. |
LayersRgb | Specifies the color of less important shaded geometry when See-Thru Style is set to Layers. |
LayersEdges | Determines whether edges are displayed for less important shaded geometry when See-Thru Style is set to Layers. |
LayersEdgesRgb | Specifies the color of edges displayed for less important shaded geometry when See-Thru Style is set to Layers. |
LayersTranslucency | Translucency percentage applied to less important shaded geometry when See-Thru Style is set to Layers. |
ShellRgb¶
-
SessionVisualizationShadeSeeThruOptions_Struct.
ShellRgb
¶ Specifies the color of less important shaded geometry when See-Thru Style is set to Shell.
-------------------------------------
Getter Method Signature
ShellRgb()
Returns: Return type: NXOpen.Preferences.SessionVisualizationShadeRgb_Struct
-------------------------------------
Setter Method
Signature
ShellRgb(value)
Parameters: value ( NXOpen.Preferences.SessionVisualizationShadeRgb_Struct
) –
ShellEdges¶
-
SessionVisualizationShadeSeeThruOptions_Struct.
ShellEdges
¶ Determines whether edges are displayed for less important shaded geometry when See-Thru Style is set to Shell.
-------------------------------------
Getter Method Signature
ShellEdges()
Returns: Return type: NXOpen.Preferences.SessionVisualizationShadeSeeThruEdgesType
-------------------------------------
Setter Method
Signature
ShellEdges(value)
Parameters: value ( NXOpen.Preferences.SessionVisualizationShadeSeeThruEdgesType
) –
ShellEdgesRgb¶
-
SessionVisualizationShadeSeeThruOptions_Struct.
ShellEdgesRgb
¶ Specifies the color of edges displayed for less important shaded geometry when See-Thru Style is set to Shell.
-------------------------------------
Getter Method Signature
ShellEdgesRgb()
Returns: Return type: NXOpen.Preferences.SessionVisualizationShadeRgb_Struct
-------------------------------------
Setter Method
Signature
ShellEdgesRgb(value)
Parameters: value ( NXOpen.Preferences.SessionVisualizationShadeRgb_Struct
) –
ShellTranslucency¶
-
SessionVisualizationShadeSeeThruOptions_Struct.
ShellTranslucency
¶ Translucency percentage applied to less important shaded geometry when See-Thru Style is set to Shell.
-------------------------------------
Getter Method Signature
ShellTranslucency()
Returns: Return type: int -------------------------------------
Setter Method
Signature
ShellTranslucency(value)
Parameters: value (int) –
OriginalColorShellEdges¶
-
SessionVisualizationShadeSeeThruOptions_Struct.
OriginalColorShellEdges
¶ Determines whether edges are displayed for less important shaded geometry when See-Thru Style is set to Original Color Shell.
-------------------------------------
Getter Method Signature
OriginalColorShellEdges()
Returns: Return type: NXOpen.Preferences.SessionVisualizationShadeSeeThruEdgesType
-------------------------------------
Setter Method
Signature
OriginalColorShellEdges(value)
Parameters: value ( NXOpen.Preferences.SessionVisualizationShadeSeeThruEdgesType
) –
OriginalColorShellEdgesRgb¶
-
SessionVisualizationShadeSeeThruOptions_Struct.
OriginalColorShellEdgesRgb
¶ Specifies the color of edges displayed for less important shaded geometry when See-Thru Style is set to Original Color Shell.
-------------------------------------
Getter Method Signature
OriginalColorShellEdgesRgb()
Returns: Return type: NXOpen.Preferences.SessionVisualizationShadeRgb_Struct
-------------------------------------
Setter Method
Signature
OriginalColorShellEdgesRgb(value)
Parameters: value ( NXOpen.Preferences.SessionVisualizationShadeRgb_Struct
) –
OriginalColorShellTranslucency¶
-
SessionVisualizationShadeSeeThruOptions_Struct.
OriginalColorShellTranslucency
¶ Translucency percentage applied to less important shaded geometry when See-Thru Style is set to Original Color Shell.
-------------------------------------
Getter Method Signature
OriginalColorShellTranslucency()
Returns: Return type: int -------------------------------------
Setter Method
Signature
OriginalColorShellTranslucency(value)
Parameters: value (int) –
LayersRgb¶
-
SessionVisualizationShadeSeeThruOptions_Struct.
LayersRgb
¶ Specifies the color of less important shaded geometry when See-Thru Style is set to Layers.
-------------------------------------
Getter Method Signature
LayersRgb()
Returns: Return type: NXOpen.Preferences.SessionVisualizationShadeRgb_Struct
-------------------------------------
Setter Method
Signature
LayersRgb(value)
Parameters: value ( NXOpen.Preferences.SessionVisualizationShadeRgb_Struct
) –
LayersEdges¶
-
SessionVisualizationShadeSeeThruOptions_Struct.
LayersEdges
¶ Determines whether edges are displayed for less important shaded geometry when See-Thru Style is set to Layers.
-------------------------------------
Getter Method Signature
LayersEdges()
Returns: Return type: NXOpen.Preferences.SessionVisualizationShadeSeeThruEdgesType
-------------------------------------
Setter Method
Signature
LayersEdges(value)
Parameters: value ( NXOpen.Preferences.SessionVisualizationShadeSeeThruEdgesType
) –
LayersEdgesRgb¶
-
SessionVisualizationShadeSeeThruOptions_Struct.
LayersEdgesRgb
¶ Specifies the color of edges displayed for less important shaded geometry when See-Thru Style is set to Layers.
-------------------------------------
Getter Method Signature
LayersEdgesRgb()
Returns: Return type: NXOpen.Preferences.SessionVisualizationShadeRgb_Struct
-------------------------------------
Setter Method
Signature
LayersEdgesRgb(value)
Parameters: value ( NXOpen.Preferences.SessionVisualizationShadeRgb_Struct
) –
LayersTranslucency¶
-
SessionVisualizationShadeSeeThruOptions_Struct.
LayersTranslucency
¶ Translucency percentage applied to less important shaded geometry when See-Thru Style is set to Layers.
-------------------------------------
Getter Method Signature
LayersTranslucency()
Returns: Return type: int -------------------------------------
Setter Method
Signature
LayersTranslucency(value)
Parameters: value (int) –