SessionVisualizationHighQualityImageImageSizeType Enumeration¶
NXOpen.Preferences.SessionVisualizationHighQualityImage.ImageSizeType is an alias for NXOpen.Preferences.SessionVisualizationHighQualityImageImageSizeType
-
class
NXOpen.Preferences.
SessionVisualizationHighQualityImageImageSizeType
¶ Bases:
object
The size at which to generate a High Quality Image.
Enum Members
Enum Member Enum Member Description FillView AnsiA AnsiB AnsiC AnsiD AnsiE IsoA4 IsoA3 IsoA2 IsoA1 IsoA0 UserDefined TrueSize -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-