SessionPdmUnpopulatedBehaviourType Enumeration¶
NXOpen.Preferences.SessionPdm.UnpopulatedBehaviourType is an alias for NXOpen.Preferences.SessionPdmUnpopulatedBehaviourType
-
class
NXOpen.Preferences.
SessionPdmUnpopulatedBehaviourType
¶ Bases:
object
Options for when to add NX datasets upon loading an unpopulated part in the PDM system
Enum Members
Enum Member Enum Member Description OnSave ModifiedPrompt ModifiedNoPrompt Never PreNx4 -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-