SessionModelingSplineDefaultActionTypes Enumeration¶
NXOpen.Preferences.SessionModeling.SplineDefaultActionTypes is an alias for NXOpen.Preferences.SessionModelingSplineDefaultActionTypes
-
class
NXOpen.Preferences.
SessionModelingSplineDefaultActionTypes
¶ Bases:
object
Specifies the command that should be invoked when double-clicking on a spline.
The option applies to non-associative splines and Studio Spline features in the Shape Studio application only. .. versionadded:: NX7.0.0
Enum Members
Enum Member Enum Member Description StudioSpline Specifies Studio Spline for editing a splineXform Specifies X-form for editing a spline-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-