SessionModelingLinkedAndExtractedGeometryPropertiesInheritance Enumeration¶
NXOpen.Preferences.SessionModeling.LinkedAndExtractedGeometryPropertiesInheritance is an alias for NXOpen.Preferences.SessionModelingLinkedAndExtractedGeometryPropertiesInheritance
-
class
NXOpen.Preferences.
SessionModelingLinkedAndExtractedGeometryPropertiesInheritance
¶ Bases:
object
Describes whether the display of linked and extracted geometry properties inherits from parent object or part default
Enum Members
Enum Member Enum Member Description ParentObject Indicates that display of linked and extracted geometry properties inherits from parent objectPartDefault Indicates that display of linked and extracted geometry properties inherits from part default-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-