SessionModelingCurveFitMethodType Enumeration¶
NXOpen.Preferences.SessionModeling.CurveFitMethodType is an alias for NXOpen.Preferences.SessionModelingCurveFitMethodType
-
class
NXOpen.Preferences.
SessionModelingCurveFitMethodType
¶ Bases:
object
Describes whether the Curve Fit Method type is selected as cubic or quintic or advanced
Enum Members
Enum Member Enum Member Description Cubic Indicates the Curve Fit Method type is cubicQuintic Indicates the Curve Fit Method type is quinticAdvanced Indicates the Curve Fit Method type is advanced-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-