SessionDrafting Class¶
-
class
NXOpen.Preferences.
SessionDrafting
¶ Bases:
object
Represents the set of Drafting preferences applicable to entire session
To obtain an instance of this class, refer to
NXOpen.Preferences.SessionPreferences
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
AutomaticCustomSymbolUpdate | Returns or sets the automatic update drafting preferences for custom symbol |
DynamicAlignment | Returns or sets the dynamic alignment flag. |
ExtractedEdgeFaceDisplay | Returns or sets the extracted edge face display |
ForcedWelcomeMode | Returns or sets the Drafting Welcome mode, for autotests only |
GridObject | Returns or sets the drafting grid object. |
LoadComponentOnFacetedViewSelection | Returns or sets the load on selection flag |
LoadComponentOnFacetedViewUpdate | Returns or sets the load on update flag |
Methods¶
Enumerations¶
SessionDraftingAnnotationStyleType Enumeration | Describes the available types for annotation style preference |
SessionDraftingEdgeFaceDisplayType Enumeration | Describes the available edge face display types |
SessionDraftingGridObjectType Enumeration | Describes the available grid objects |
Property Detail¶
AutomaticCustomSymbolUpdate¶
-
SessionDrafting.
AutomaticCustomSymbolUpdate
¶ Returns or sets the automatic update drafting preferences for custom symbol
-------------------------------------
Getter Method
Signature
AutomaticCustomSymbolUpdate()
Returns: Return type: bool New in version NX8.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
AutomaticCustomSymbolUpdate(automaticUpdateOption)
Parameters: automaticUpdateOption (bool) – New in version NX8.0.1.
License requirements: None.
DynamicAlignment¶
-
SessionDrafting.
DynamicAlignment
¶ Returns or sets the dynamic alignment flag.
-------------------------------------
Getter Method
Signature
DynamicAlignment()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DynamicAlignment(dynamicAlignment)
Parameters: dynamicAlignment (bool) – New in version NX3.0.0.
License requirements: None.
ExtractedEdgeFaceDisplay¶
-
SessionDrafting.
ExtractedEdgeFaceDisplay
¶ Returns or sets the extracted edge face display
-------------------------------------
Getter Method
Signature
ExtractedEdgeFaceDisplay()
Returns: Return type: NXOpen.Preferences.SessionDraftingEdgeFaceDisplayType
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtractedEdgeFaceDisplay(extractedEdgeFaceDisplay)
Parameters: extractedEdgeFaceDisplay ( NXOpen.Preferences.SessionDraftingEdgeFaceDisplayType
) –New in version NX3.0.0.
License requirements: None.
ForcedWelcomeMode¶
-
SessionDrafting.
ForcedWelcomeMode
¶ Returns or sets the Drafting Welcome mode, for autotests only
-------------------------------------
Getter Method
Signature
ForcedWelcomeMode()
Returns: 0: no welcome, 1: ALWAYS welcome, 2: default Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ForcedWelcomeMode(enterWelcomeMode)
Parameters: enterWelcomeMode (int) – 0: do NOT use welcome, 1: ALWAYS use welcome New in version NX8.0.0.
License requirements: None.
GridObject¶
-
SessionDrafting.
GridObject
¶ Returns or sets the drafting grid object.
-------------------------------------
Getter Method
Signature
GridObject()
Returns: Return type: NXOpen.Preferences.SessionDraftingGridObjectType
New in version NX6.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
GridObject(drawingGridObject)
Parameters: drawingGridObject ( NXOpen.Preferences.SessionDraftingGridObjectType
) –New in version NX6.0.2.
License requirements: None.
LoadComponentOnFacetedViewSelection¶
-
SessionDrafting.
LoadComponentOnFacetedViewSelection
¶ Returns or sets the load on selection flag
-------------------------------------
Getter Method
Signature
LoadComponentOnFacetedViewSelection()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LoadComponentOnFacetedViewSelection(loadComponentOnFacetedViewSelection)
Parameters: loadComponentOnFacetedViewSelection (bool) – New in version NX3.0.0.
License requirements: None.
LoadComponentOnFacetedViewUpdate¶
-
SessionDrafting.
LoadComponentOnFacetedViewUpdate
¶ Returns or sets the load on update flag
-------------------------------------
Getter Method
Signature
LoadComponentOnFacetedViewUpdate()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LoadComponentOnFacetedViewUpdate(loadComponentOnFacetedViewUpdate)
Parameters: loadComponentOnFacetedViewUpdate (bool) – New in version NX3.0.0.
License requirements: None.