RoutingPathRadiusUnits Enumeration¶
NXOpen.Preferences.RoutingPath.RadiusUnits is an alias for NXOpen.Preferences.RoutingPathRadiusUnits
-
class
NXOpen.Preferences.
RoutingPathRadiusUnits
¶ Bases:
object
Describes units of specified radius value [JA_ROUTE_PATH_PREFS_radius_method_radius only].
Enum Members
Enum Member Enum Member Description None Unspecified. Use units of part file.Inches Use inch unitsMillimeters Use metric (mm) units-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-