RoutingPathCreateTangency Enumeration¶
NXOpen.Preferences.RoutingPath.CreateTangency is an alias for NXOpen.Preferences.RoutingPathCreateTangency
-
class
NXOpen.Preferences.
RoutingPathCreateTangency
¶ Bases:
object
Should new splines form tangencies with existing splines when they’re created?
Enum Members
Enum Member Enum Member Description False Do not merge duplicate RCPs.True Merge duplicate RCPs.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-