RoutingPathChainMethod Enumeration¶
NXOpen.Preferences.RoutingPath.ChainMethod is an alias for NXOpen.Preferences.RoutingPathChainMethod
-
class
NXOpen.Preferences.
RoutingPathChainMethod
¶ Bases:
object
Path curve chaining methods
Enum Members
Enum Member Enum Member Description NoBranch Curves must be mono-connectedContinuous Tangents must match at each connectionTangent Use curve with closest tangent when searchingCycle Return all chainsMinDist Chain with minimum path lengthMaxDist Chain with maximum path length-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-