RoutingPartLibraryColumn_Struct Struct¶
NXOpen.Preferences.RoutingPartLibrary.Column is an alias for NXOpen.Preferences.RoutingPartLibraryColumn_Struct
-
class
NXOpen.Preferences.
RoutingPartLibraryColumn_Struct
¶ Bases:
object
Part table column type.
Fields¶
Field | Description |
---|---|
Name | Column name. |
Hidden | Whether or not the column is used for selection in the specify item dialog. |
Type | The value type the column stores. |
Name¶
-
RoutingPartLibraryColumn_Struct.
Name
¶ Column name.
PART_NUMBER is the index column for all part tables.
-------------------------------------
Getter Method Signature
Name()
Returns: Return type: str -------------------------------------
Setter Method
Signature
Name(value)
Parameters: value (str) –
Type¶
-
RoutingPartLibraryColumn_Struct.
Type
¶ The value type the column stores.
-------------------------------------
Getter Method Signature
Type()
Returns: Return type: NXOpen.Preferences.RoutingPartLibraryColumnType
-------------------------------------
Setter Method
Signature
Type(value)
Parameters: value ( NXOpen.Preferences.RoutingPartLibraryColumnType
) –