RoutingPartFabricationNumbering Enumeration¶
NXOpen.Preferences.RoutingPart.FabricationNumbering is an alias for NXOpen.Preferences.RoutingPartFabricationNumbering
-
class
NXOpen.Preferences.
RoutingPartFabricationNumbering
¶ Bases:
object
The fabrication numbering methods available for the Routing bill of material.
Enum Members
Enum Member Enum Member Description Sequence Sequential numbering of fabrications in the parts list.Original Use the fabrication number in the parts list.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-