RoutingLogical Class¶
-
class
NXOpen.Preferences.
RoutingLogical
¶ Bases:
object
The RoutingLogical object stores a set of route logical preferences.
To obtain an instance of this class, refer to
NXOpen.Preferences.RoutingApplicationView
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
FlowArrowParameterA | Returns or sets the application view flow arrow parameter A |
FlowArrowParameterB | Returns or sets the application view flow arrow parameter B |
FlowArrowType | Returns or sets the application view flow arrow type |
Methods¶
Enumerations¶
RoutingLogicalFlowArrowEnumType Enumeration | How to create terminal segments (if creating terminal segments). |
Property Detail¶
FlowArrowParameterA¶
-
RoutingLogical.
FlowArrowParameterA
¶ Returns or sets the application view flow arrow parameter A
-------------------------------------
Getter Method
Signature
FlowArrowParameterA()
Returns: Return type: float New in version NX4.0.0.
License requirements: routing_pid (“Routing PID”)
-------------------------------------
Setter Method
Signature
FlowArrowParameterA(flowArrowParameterA)
Parameters: flowArrowParameterA (float) – New in version NX4.0.0.
License requirements: routing_pid (“Routing PID”)
FlowArrowParameterB¶
-
RoutingLogical.
FlowArrowParameterB
¶ Returns or sets the application view flow arrow parameter B
-------------------------------------
Getter Method
Signature
FlowArrowParameterB()
Returns: Return type: float New in version NX4.0.0.
License requirements: routing_pid (“Routing PID”)
-------------------------------------
Setter Method
Signature
FlowArrowParameterB(flowArrowParameterB)
Parameters: flowArrowParameterB (float) – New in version NX4.0.0.
License requirements: routing_pid (“Routing PID”)
FlowArrowType¶
-
RoutingLogical.
FlowArrowType
¶ Returns or sets the application view flow arrow type
-------------------------------------
Getter Method
Signature
FlowArrowType()
Returns: Return type: NXOpen.Preferences.RoutingLogicalFlowArrowEnumType
New in version NX4.0.0.
License requirements: routing_pid (“Routing PID”)
-------------------------------------
Setter Method
Signature
FlowArrowType(flowArrowType)
Parameters: flowArrowType ( NXOpen.Preferences.RoutingLogicalFlowArrowEnumType
) –New in version NX4.0.0.
License requirements: routing_pid (“Routing PID”)