RoutingElectrical Class¶
-
class
NXOpen.Preferences.
RoutingElectrical
¶ Bases:
object
The RoutingElectrical object stores a set of route electrical preferences.
A valid application view file is necessary to get values other than defaults for the electrical preferences. To obtain an instance of this class, refer to
NXOpen.Preferences.RoutingApplicationView
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
AutoRouteStockStyle | Returns or sets the option to Auto Route using centerline stock style (i. |
AutomaticRouteLevel | Returns or sets the level at which to automatically route a path. |
BundleColor | Returns or sets the default bundle color. |
ComponentMatchMethod | Returns or sets the component match option for automatic/manual component assignment. |
CreateTerminalsOption | Returns or sets the create terminals option. |
DefaultJumperLength | Returns or sets the default length of a jumper wire. |
ExportFormatInLegacyFile | Returns or sets the option to export the format at the top of a legacy routelist file. |
FormboardSynchronizationLengthTolerance | Returns or sets the default segment length tolerance to use for Formboard Synchronization. |
HighlightWire | Returns or sets the option to highlight a wire in the connection list navigator. |
RecordNetlistHistory | Returns or sets the option to record import and export activity in the Connection and Component Lists. |
ReportRouteErrors | Returns or sets the option to report auto/manual route errors to the listing window. |
StandaloneFilterFormatFile | Returns or sets the option to export the XML routelist data with the formats and filters information separately. |
TerminalSegmentSolidDisplay | Returns or sets the terminal segment solid display option |
Methods¶
Method | Description |
---|---|
GetComponentMatchColumnHeading | Gets the column name of the component list used for component matching if the method is attribute matching. |
GetComponentMatchComponentAttributeTitle | Gets the component attribute name used for component matching if the method is attribute matching. |
GetDefaultHarnessName | Gets the default harness name. |
GetFilterBlankingAttribute | Gets the Rlist_Filter_Blanking_Attribute. |
GetFilterFormatFileName | Gets the file name for the stand alone XML filters and formats file. |
GetFormboardFrameSizes | Gets the formboard frame sizes currently specified within the Routing Electrical application. |
SetComponentMatchColumnHeading | Sets the column name of the component list used for component matching if the method is attribute matching. |
SetComponentMatchComponentAttributeTitle | Sets the component attribute name used for component matching if the method is attribute matching. |
SetDefaultHarnessName | Sets the default harness name |
SetFilterBlankingAttribute | Sets the Rlist_Filter_Blanking_Attribute. |
SetFilterFormatFileName | Sets the file name for the stand alone XML filters and formats file. |
SetFormboardFrameSizes | Sets a formboard frame size. |
Enumerations¶
RoutingElectricalComponentMatchType Enumeration | Manual/Auto Assign component uses the component match method to determine which component(s) are candidates for assignment to a component list record. |
RoutingElectricalCreateTerminalsType Enumeration | How to create terminal segments (if creating terminal segments). |
Property Detail¶
AutoRouteStockStyle¶
-
RoutingElectrical.
AutoRouteStockStyle
¶ Returns or sets the option to Auto Route using centerline stock style (i.
- none) or simple stock style.
-------------------------------------
Getter Method
Signature
AutoRouteStockStyle()
Returns: Will be either NXOpen.Routing.StockStyle.None
) orNXOpen.Routing.StockStyle.Simple
). :rtype:NXOpen.Routing.StockStyle
New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
AutoRouteStockStyle(stockStyle)
Parameters: stockStyle ( NXOpen.Routing.StockStyle
) – Must be eitherNXOpen.Routing.StockStyle.None
) orNXOpen.Routing.StockStyle.Simple
).New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
AutomaticRouteLevel¶
-
RoutingElectrical.
AutomaticRouteLevel
¶ Returns or sets the level at which to automatically route a path.
-------------------------------------
Getter Method
Signature
AutomaticRouteLevel()
Returns: Return type: bool New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
AutomaticRouteLevel(isPinLevelRoute)
Parameters: isPinLevelRoute (bool) – New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
BundleColor¶
-
RoutingElectrical.
BundleColor
¶ Returns or sets the default bundle color.
-------------------------------------
Getter Method
Signature
BundleColor()
Returns: Return type: int New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
BundleColor(bundleColor)
Parameters: bundleColor (int) – New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
ComponentMatchMethod¶
-
RoutingElectrical.
ComponentMatchMethod
¶ Returns or sets the component match option for automatic/manual component assignment.
-------------------------------------
Getter Method
Signature
ComponentMatchMethod()
Returns: Return type: NXOpen.Preferences.RoutingElectricalComponentMatchType
New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
ComponentMatchMethod(componentMatchMethod)
Parameters: componentMatchMethod ( NXOpen.Preferences.RoutingElectricalComponentMatchType
) –New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
CreateTerminalsOption¶
-
RoutingElectrical.
CreateTerminalsOption
¶ Returns or sets the create terminals option.
-------------------------------------
Getter Method
Signature
CreateTerminalsOption()
Returns: Return type: NXOpen.Preferences.RoutingElectricalCreateTerminalsType
New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
CreateTerminalsOption(createTerminalsOption)
Parameters: createTerminalsOption ( NXOpen.Preferences.RoutingElectricalCreateTerminalsType
) –New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
DefaultJumperLength¶
-
RoutingElectrical.
DefaultJumperLength
¶ Returns or sets the default length of a jumper wire.
-------------------------------------
Getter Method
Signature
DefaultJumperLength()
Returns: Return type: str New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
DefaultJumperLength(defaultJumperLength)
Parameters: defaultJumperLength (str) – New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
ExportFormatInLegacyFile¶
-
RoutingElectrical.
ExportFormatInLegacyFile
¶ Returns or sets the option to export the format at the top of a legacy routelist file.
-------------------------------------
Getter Method
Signature
ExportFormatInLegacyFile()
Returns: Return type: bool New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
ExportFormatInLegacyFile(exportFormat)
Parameters: exportFormat (bool) – New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
FormboardSynchronizationLengthTolerance¶
-
RoutingElectrical.
FormboardSynchronizationLengthTolerance
¶ Returns or sets the default segment length tolerance to use for Formboard Synchronization.
-------------------------------------
Getter Method
Signature
FormboardSynchronizationLengthTolerance()
Returns: Return type: float New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
FormboardSynchronizationLengthTolerance(segmentLengthTolerance)
Parameters: segmentLengthTolerance (float) – New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
HighlightWire¶
-
RoutingElectrical.
HighlightWire
¶ Returns or sets the option to highlight a wire in the connection list navigator.
-------------------------------------
Getter Method
Signature
HighlightWire()
Returns: Return type: bool New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
HighlightWire(highlightWire)
Parameters: highlightWire (bool) – New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
RecordNetlistHistory¶
-
RoutingElectrical.
RecordNetlistHistory
¶ Returns or sets the option to record import and export activity in the Connection and Component Lists.
-------------------------------------
Getter Method
Signature
RecordNetlistHistory()
Returns: Return type: bool New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
RecordNetlistHistory(recordNetlistHistory)
Parameters: recordNetlistHistory (bool) – Should Routing record the netlist history? New in version NX6.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
ReportRouteErrors¶
-
RoutingElectrical.
ReportRouteErrors
¶ Returns or sets the option to report auto/manual route errors to the listing window.
-------------------------------------
Getter Method
Signature
ReportRouteErrors()
Returns: Return type: bool New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
ReportRouteErrors(reportRouteErrors)
Parameters: reportRouteErrors (bool) – New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
StandaloneFilterFormatFile¶
-
RoutingElectrical.
StandaloneFilterFormatFile
¶ Returns or sets the option to export the XML routelist data with the formats and filters information separately.
-------------------------------------
Getter Method
Signature
StandaloneFilterFormatFile()
Returns: Return type: bool New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
StandaloneFilterFormatFile(standaloneFilterFormatFile)
Parameters: standaloneFilterFormatFile (bool) – New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
TerminalSegmentSolidDisplay¶
-
RoutingElectrical.
TerminalSegmentSolidDisplay
¶ Returns or sets the terminal segment solid display option
-------------------------------------
Getter Method
Signature
TerminalSegmentSolidDisplay()
Returns: Return type: bool New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
TerminalSegmentSolidDisplay(terminalSegmentSolid)
Parameters: terminalSegmentSolid (bool) – New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
Method Detail¶
GetComponentMatchColumnHeading¶
-
RoutingElectrical.
GetComponentMatchColumnHeading
¶ Gets the column name of the component list used for component matching if the method is attribute matching.
Signature
GetComponentMatchColumnHeading()
Returns: Return type: str New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetComponentMatchComponentAttributeTitle¶
-
RoutingElectrical.
GetComponentMatchComponentAttributeTitle
¶ Gets the component attribute name used for component matching if the method is attribute matching.
Signature
GetComponentMatchComponentAttributeTitle()
Returns: Return type: str New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetDefaultHarnessName¶
-
RoutingElectrical.
GetDefaultHarnessName
¶ Gets the default harness name.
The default harness name replaces the Harness field value of any records in an imported connection/component list that are empty. A blank string in the Default_Harness_Name element below replaces blank Harness fields with the leaf name of the work part.
Signature
GetDefaultHarnessName()
Returns: Return type: str New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetFilterBlankingAttribute¶
-
RoutingElectrical.
GetFilterBlankingAttribute
¶ Gets the Rlist_Filter_Blanking_Attribute.
Signature
GetFilterBlankingAttribute()
Returns: Return type: str New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetFilterFormatFileName¶
-
RoutingElectrical.
GetFilterFormatFileName
¶ Gets the file name for the stand alone XML filters and formats file.
Signature
GetFilterFormatFileName()
Returns: Return type: str New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetFormboardFrameSizes¶
-
RoutingElectrical.
GetFormboardFrameSizes
¶ Gets the formboard frame sizes currently specified within the Routing Electrical application.
Formboard frame sizes are character strings are of the form Height x Length (units).
Units can be “in” or “mm” (case insensitive).
The Height, Length and units fields of the string are separated by one of the following separator characters:
“x”, “X”, any whitespace, ”:” (colon), or a ”,” (comma)
Signature
GetFormboardFrameSizes()
Returns: Return type: list of str New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SetComponentMatchColumnHeading¶
-
RoutingElectrical.
SetComponentMatchColumnHeading
¶ Sets the column name of the component list used for component matching if the method is attribute matching.
Signature
SetComponentMatchColumnHeading(columnHeading)
Parameters: columnHeading (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SetComponentMatchComponentAttributeTitle¶
-
RoutingElectrical.
SetComponentMatchComponentAttributeTitle
¶ Sets the component attribute name used for component matching if the method is attribute matching.
Signature
SetComponentMatchComponentAttributeTitle(componentAttributeTitle)
Parameters: componentAttributeTitle (str) – New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SetDefaultHarnessName¶
-
RoutingElectrical.
SetDefaultHarnessName
¶ Sets the default harness name
Signature
SetDefaultHarnessName(defaultHarnessName)
Parameters: defaultHarnessName (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SetFilterBlankingAttribute¶
-
RoutingElectrical.
SetFilterBlankingAttribute
¶ Sets the Rlist_Filter_Blanking_Attribute.
Signature
SetFilterBlankingAttribute(attributeName)
Parameters: attributeName (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SetFilterFormatFileName¶
-
RoutingElectrical.
SetFilterFormatFileName
¶ Sets the file name for the stand alone XML filters and formats file.
Signature
SetFilterFormatFileName(filterFormatFileName)
Parameters: filterFormatFileName (str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
SetFormboardFrameSizes¶
-
RoutingElectrical.
SetFormboardFrameSizes
¶ Sets a formboard frame size.
Signature
SetFormboardFrameSizes(frameSizes)
Parameters: frameSizes (list of str) – NOTE: The full Unicode character set is not supported for this parameter. New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)