PartVisualizationEmphasisWireframeBlendOptions_Struct Struct¶
NXOpen.Preferences.PartVisualizationEmphasis.WireframeBlendOptions is an alias for NXOpen.Preferences.PartVisualizationEmphasisWireframeBlendOptions_Struct
-
class
NXOpen.Preferences.
PartVisualizationEmphasisWireframeBlendOptions_Struct
¶ Bases:
object
Specifies options that control the color-blending effect used to de-emphasize wireframe geometry.
Fields¶
Field | Description |
---|---|
BlendColor | the de-emphasis color that is blended with object colors to de-emphasize wireframe geometry. |
BlendPercentage | the percentage of the de-emphasis color that is blended with object colors to de-emphasize wireframe geometry It is a value between 10 and 100. |
BlendColor¶
-
PartVisualizationEmphasisWireframeBlendOptions_Struct.
BlendColor
¶ the de-emphasis color that is blended with object colors to de-emphasize wireframe geometry.
-------------------------------------
Getter Method Signature
BlendColor()
Returns: Return type: Id -------------------------------------
Setter Method
Signature
BlendColor(value)
Parameters: value (Id) –
BlendPercentage¶
-
PartVisualizationEmphasisWireframeBlendOptions_Struct.
BlendPercentage
¶ the percentage of the de-emphasis color that is blended with object colors to de-emphasize wireframe geometry It is a value between 10 and 100.
-------------------------------------
Getter Method Signature
BlendPercentage()
Returns: Return type: int -------------------------------------
Setter Method
Signature
BlendPercentage(value)
Parameters: value (int) –