PartVisualizationEmphasisOriginalColorShellOptions_Struct Struct¶
NXOpen.Preferences.PartVisualizationEmphasis.OriginalColorShellOptions is an alias for NXOpen.Preferences.PartVisualizationEmphasisOriginalColorShellOptions_Struct
-
class
NXOpen.Preferences.
PartVisualizationEmphasisOriginalColorShellOptions_Struct
¶ Bases:
object
Specifies options that control the appearance of de-emphasized shaded geometry when the See-Thru style is set to Original Color Shell.
Fields¶
Field | Description |
---|---|
Edges | whether or not edges are displayed for de-emphasized shaded geometry when the See-Thru style is set to Original Color Shell. |
EdgesRgb | the color of edges displayed for de-emphasized shaded geometry when the See-Thru style is set to Original Color Shell. |
Translucency | the translucency of de-emphasized shaded geometry when the See-Thru style is set to Original Color Shell. |
Edges¶
-
PartVisualizationEmphasisOriginalColorShellOptions_Struct.
Edges
¶ whether or not edges are displayed for de-emphasized shaded geometry when the See-Thru style is set to Original Color Shell.
-------------------------------------
Getter Method Signature
Edges()
Returns: Return type: NXOpen.Preferences.PartVisualizationEmphasisEdgesType
-------------------------------------
Setter Method
Signature
Edges(value)
Parameters: value ( NXOpen.Preferences.PartVisualizationEmphasisEdgesType
) –
EdgesRgb¶
-
PartVisualizationEmphasisOriginalColorShellOptions_Struct.
EdgesRgb
¶ the color of edges displayed for de-emphasized shaded geometry when the See-Thru style is set to Original Color Shell.
-------------------------------------
Getter Method Signature
EdgesRgb()
Returns: Return type: NXOpen.NXColorRgb_Struct
-------------------------------------
Setter Method
Signature
EdgesRgb(value)
Parameters: value ( NXOpen.NXColorRgb_Struct
) –
Translucency¶
-
PartVisualizationEmphasisOriginalColorShellOptions_Struct.
Translucency
¶ the translucency of de-emphasized shaded geometry when the See-Thru style is set to Original Color Shell.
It is a percentage value between 30 and 100.
-------------------------------------
Getter Method Signature
Translucency()
Returns: Return type: int -------------------------------------
Setter Method
Signature
Translucency(value)
Parameters: value (int) –