PartVisualizationColorSetting Class¶
-
class
NXOpen.Preferences.
PartVisualizationColorSetting
¶ Bases:
object
Represents the set of visualization preferences under color setting tab applicable to part
To obtain an instance of this class, refer to
NXOpen.Preferences.PartPreferences
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
AttentionColor | Returns or sets the color that an HD3D objects associated objects are highlighted with when the HD3D object is selected. |
DeEmphasisBlendColor | Returns or sets the de-emphasis color that is blended with object colors to de-emphasize objects |
DeEmphasisBlendPercentage | Returns or sets the percentage of the de-emphasis color that is blended with object colors to de-emphasize objects |
HandleActiveColor | Returns or sets the color of active handles. |
HandleColor | Returns or sets the color of handles. |
HandleOrientxpressColor | Returns or sets the color of the OrientXpress handle. |
HandlePreselectionColor | Returns or sets the preselection color of handles. |
HandleSelectionColor | Returns or sets the selection color of handles. |
HiddenGeometryColor | Returns or sets the color of hidden geometry. |
MonochromeBackgroundColor | Returns or sets the monochrome background color |
MonochromeDisplay | Returns or sets the monochrome display flag. |
MonochromeForegroundColor | Returns or sets the monochrome foreground color. |
MonochromePreselectionColor | Returns or sets the monochrome color for preselected objects |
MonochromeSelectionColor | Returns or sets the monochrome selection_color. |
PreselectionColor | Returns or sets the preselection color. |
RandomColorDisplay | Returns or sets the random color display selection. |
RandomColorDisplayOption | Returns or sets the random color display flag. |
SelectionColor | Returns or sets the selection color. |
ShowWidths | Returns or sets the show widths flag. |
Methods¶
Method | Description |
---|---|
ShuffleRandomColor | Allows user to shuffle the Random color |
Enumerations¶
PartVisualizationColorSettingRandomColorDisplayFor Enumeration | Describes whether the random color display is applicable for faces or bodies |
Property Detail¶
AttentionColor¶
-
PartVisualizationColorSetting.
AttentionColor
¶ Returns or sets the color that an HD3D objects associated objects are highlighted with when the HD3D object is selected.
The color must be in the range of 1 to 216 inclusive.
-------------------------------------
Getter Method
Signature
AttentionColor()
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AttentionColor(attentionColor)
Parameters: attentionColor (int) – New in version NX7.0.0.
License requirements: None.
DeEmphasisBlendColor¶
-
PartVisualizationColorSetting.
DeEmphasisBlendColor
¶ Returns or sets the de-emphasis color that is blended with object colors to de-emphasize objects
-------------------------------------
Getter Method
Signature
DeEmphasisBlendColor()
Returns: Return type: int New in version NX6.0.0.
Deprecated since version NX8.5.0: Use
Preferences.PartVisualizationEmphasis.GetWireframeBlendOptions
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
DeEmphasisBlendColor(blendColor)
Parameters: blendColor (int) – New in version NX6.0.0.
Deprecated since version NX8.5.0: Use
Preferences.PartVisualizationEmphasis.SetWireframeBlendOptions
instead.License requirements: None.
DeEmphasisBlendPercentage¶
-
PartVisualizationColorSetting.
DeEmphasisBlendPercentage
¶ Returns or sets the percentage of the de-emphasis color that is blended with object colors to de-emphasize objects
-------------------------------------
Getter Method
Signature
DeEmphasisBlendPercentage()
Returns: Return type: int New in version NX6.0.0.
Deprecated since version NX8.5.0: Use
Preferences.PartVisualizationEmphasis.GetWireframeBlendOptions
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
DeEmphasisBlendPercentage(blendPercentage)
Parameters: blendPercentage (int) – New in version NX6.0.0.
Deprecated since version NX8.5.0: Use
Preferences.PartVisualizationEmphasis.SetWireframeBlendOptions
instead.License requirements: None.
HandleActiveColor¶
-
PartVisualizationColorSetting.
HandleActiveColor
¶ Returns or sets the color of active handles.
-------------------------------------
Getter Method
Signature
HandleActiveColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HandleActiveColor(handleActiveColor)
Parameters: handleActiveColor (Id) – New in version NX7.5.0.
License requirements: None.
HandleColor¶
-
PartVisualizationColorSetting.
HandleColor
¶ Returns or sets the color of handles.
-------------------------------------
Getter Method
Signature
HandleColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HandleColor(handleColor)
Parameters: handleColor (Id) – New in version NX7.5.0.
License requirements: None.
HandleOrientxpressColor¶
-
PartVisualizationColorSetting.
HandleOrientxpressColor
¶ Returns or sets the color of the OrientXpress handle.
-------------------------------------
Getter Method
Signature
HandleOrientxpressColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HandleOrientxpressColor(handleOrientxpressColor)
Parameters: handleOrientxpressColor (Id) – New in version NX7.5.0.
License requirements: None.
HandlePreselectionColor¶
-
PartVisualizationColorSetting.
HandlePreselectionColor
¶ Returns or sets the preselection color of handles.
-------------------------------------
Getter Method
Signature
HandlePreselectionColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HandlePreselectionColor(handlePreselectionColor)
Parameters: handlePreselectionColor (Id) – New in version NX7.5.0.
License requirements: None.
HandleSelectionColor¶
-
PartVisualizationColorSetting.
HandleSelectionColor
¶ Returns or sets the selection color of handles.
-------------------------------------
Getter Method
Signature
HandleSelectionColor()
Returns: Return type: Id New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HandleSelectionColor(handleSelectionColor)
Parameters: handleSelectionColor (Id) – New in version NX7.5.0.
License requirements: None.
MonochromeBackgroundColor¶
-
PartVisualizationColorSetting.
MonochromeBackgroundColor
¶ Returns or sets the monochrome background color
-------------------------------------
Getter Method
Signature
MonochromeBackgroundColor()
Returns: Return type: int New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MonochromeBackgroundColor(monochromeBackgroundColor)
Parameters: monochromeBackgroundColor (int) – New in version NX3.0.0.
License requirements: None.
MonochromeDisplay¶
-
PartVisualizationColorSetting.
MonochromeDisplay
¶ Returns or sets the monochrome display flag.
If true it turns on the monochrome display options. Monochrome display also applies to Expanded drawing views.
-------------------------------------
Getter Method
Signature
MonochromeDisplay()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MonochromeDisplay(monochromeDisplay)
Parameters: monochromeDisplay (bool) – New in version NX3.0.0.
License requirements: None.
MonochromeForegroundColor¶
-
PartVisualizationColorSetting.
MonochromeForegroundColor
¶ Returns or sets the monochrome foreground color.
Monochrome color for all displayable objects, view borders, and view names.
-------------------------------------
Getter Method
Signature
MonochromeForegroundColor()
Returns: Return type: int New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MonochromeForegroundColor(monochromeForegroundColor)
Parameters: monochromeForegroundColor (int) – New in version NX3.0.0.
License requirements: None.
MonochromePreselectionColor¶
-
PartVisualizationColorSetting.
MonochromePreselectionColor
¶ Returns or sets the monochrome color for preselected objects
-------------------------------------
Getter Method
Signature
MonochromePreselectionColor()
Returns: Return type: int New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MonochromePreselectionColor(monochromePreselectionColor)
Parameters: monochromePreselectionColor (int) – New in version NX3.0.0.
License requirements: None.
MonochromeSelectionColor¶
-
PartVisualizationColorSetting.
MonochromeSelectionColor
¶ Returns or sets the monochrome selection_color.
Displays all selected/highlighted objects, temporary display objects (such as coneheads, temporary text), and drawing borders in this color.
-------------------------------------
Getter Method
Signature
MonochromeSelectionColor()
Returns: Return type: int New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MonochromeSelectionColor(monochromeSelectionColor)
Parameters: monochromeSelectionColor (int) – New in version NX3.0.0.
License requirements: None.
PreselectionColor¶
-
PartVisualizationColorSetting.
PreselectionColor
¶ Returns or sets the preselection color.
Represents color of selectable objects for the current operation.
-------------------------------------
Getter Method
Signature
PreselectionColor()
Returns: Return type: int New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PreselectionColor(preselectionColor)
Parameters: preselectionColor (int) – New in version NX3.0.0.
License requirements: None.
RandomColorDisplay¶
-
PartVisualizationColorSetting.
RandomColorDisplay
¶ Returns or sets the random color display selection.
-------------------------------------
Getter Method
Signature
RandomColorDisplay()
Returns: Return type: NXOpen.Preferences.PartVisualizationColorSettingRandomColorDisplayFor
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RandomColorDisplay(randomColorDisplay)
Parameters: randomColorDisplay ( NXOpen.Preferences.PartVisualizationColorSettingRandomColorDisplayFor
) –New in version NX3.0.0.
License requirements: None.
RandomColorDisplayOption¶
-
PartVisualizationColorSetting.
RandomColorDisplayOption
¶ Returns or sets the random color display flag.
If true it provides a temporary display of unique colors per solid object.
-------------------------------------
Getter Method
Signature
RandomColorDisplayOption()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RandomColorDisplayOption(randomColorDisplayOption)
Parameters: randomColorDisplayOption (bool) – New in version NX3.0.0.
License requirements: None.
SelectionColor¶
-
PartVisualizationColorSetting.
SelectionColor
¶ Returns or sets the selection color.
Represents color of selected objects, the grid, view names and borders, and temporary points and conehead vectors.
-------------------------------------
Getter Method
Signature
SelectionColor()
Returns: Return type: int New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectionColor(selectionColor)
Parameters: selectionColor (int) – New in version NX3.0.0.
License requirements: None.
ShowWidths¶
-
PartVisualizationColorSetting.
ShowWidths
¶ Returns or sets the show widths flag.
If true, the object width attribute determines the displayed width of lines or curves used to represent an object.
-------------------------------------
Getter Method
Signature
ShowWidths()
Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowWidths(showWidths)
Parameters: showWidths (bool) – New in version NX3.0.0.
License requirements: None.