PartUserInterface Class¶
-
class
NXOpen.Preferences.
PartUserInterface
¶ Bases:
object
Represents the set of User Interface preferences applicable to entire part.
Other User Interface settings are available with
NXOpen.Preferences.SessionUserInterface
for settings applicable to session and with SessionUserInterfaceUI class for UI based User Interface Preferences To obtain an instance of this class, refer toNXOpen.Preferences.PartPreferences
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
DialogBoxDecimalPlaces | Returns or sets the dialog box decimal places |
Methods¶
Property Detail¶
DialogBoxDecimalPlaces¶
-
PartUserInterface.
DialogBoxDecimalPlaces
¶ Returns or sets the dialog box decimal places
-------------------------------------
Getter Method
Signature
DialogBoxDecimalPlaces()
Returns: Return type: int New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DialogBoxDecimalPlaces(dialogBoxDecimalPlaces)
Parameters: dialogBoxDecimalPlaces (int) – New in version NX3.0.0.
License requirements: None.