PartSheetmetalFlatPatternObjectTypeDisplay_Struct Struct¶
NXOpen.Preferences.PartSheetmetal.FlatPatternObjectTypeDisplay is an alias for NXOpen.Preferences.PartSheetmetalFlatPatternObjectTypeDisplay_Struct
-
class
NXOpen.Preferences.
PartSheetmetalFlatPatternObjectTypeDisplay_Struct
¶ Bases:
object
The members of the following structure are the display data for an object in a flat pattern drawing member view.
Fields¶
Field | Description |
---|---|
Type | Object type |
IsEnabled | Enabled status for the object type |
Color | Object color |
Layer | Object Layer |
Font | Object font |
Width | Object width |
Type¶
-
PartSheetmetalFlatPatternObjectTypeDisplay_Struct.
Type
¶ Object type
-------------------------------------
Getter Method Signature
Type()
Returns: Return type: NXOpen.Preferences.PartSheetmetalFlatPatternObjectType
-------------------------------------
Setter Method
Signature
Type(value)
Parameters: value ( NXOpen.Preferences.PartSheetmetalFlatPatternObjectType
) –
IsEnabled¶
-
PartSheetmetalFlatPatternObjectTypeDisplay_Struct.
IsEnabled
¶ Enabled status for the object type
-------------------------------------
Getter Method Signature
IsEnabled()
Returns: Return type: int -------------------------------------
Setter Method
Signature
IsEnabled(value)
Parameters: value (int) –
Color¶
-
PartSheetmetalFlatPatternObjectTypeDisplay_Struct.
Color
¶ Object color
-------------------------------------
Getter Method Signature
Color()
Returns: Return type: Id -------------------------------------
Setter Method
Signature
Color(value)
Parameters: value (Id) –
Layer¶
-
PartSheetmetalFlatPatternObjectTypeDisplay_Struct.
Layer
¶ Object Layer
-------------------------------------
Getter Method Signature
Layer()
Returns: Return type: int -------------------------------------
Setter Method
Signature
Layer(value)
Parameters: value (int) –
Font¶
-
PartSheetmetalFlatPatternObjectTypeDisplay_Struct.
Font
¶ Object font
-------------------------------------
Getter Method Signature
Font()
Returns: Return type: NXOpen.DisplayableObjectObjectFont
-------------------------------------
Setter Method
Signature
Font(value)
Parameters: value ( NXOpen.DisplayableObjectObjectFont
) –
Width¶
-
PartSheetmetalFlatPatternObjectTypeDisplay_Struct.
Width
¶ Object width
-------------------------------------
Getter Method Signature
Width()
Returns: Return type: NXOpen.DisplayableObjectObjectWidth
-------------------------------------
Setter Method
Signature
Width(value)
Parameters: value ( NXOpen.DisplayableObjectObjectWidth
) –