PartSheetmetalBendDefinitionMethodOptions Enumeration¶
NXOpen.Preferences.PartSheetmetal.BendDefinitionMethodOptions is an alias for NXOpen.Preferences.PartSheetmetalBendDefinitionMethodOptions
-
class
NXOpen.Preferences.
PartSheetmetalBendDefinitionMethodOptions
¶ Bases:
object
This enum represents the bend definition method options in preferences.
This is used to specify the bend definition method. You can choose to use a global Neutral Factor value OR a Bend Table OR a Bend Allowance Formula OR a Material Table.
New in version NX5.0.0.
Enum Members
Enum Member Enum Member Description NeutralFactorValue The neutral factor value methodBendTable The bend table methodBendAllowanceFormula The bend allowance formula methodMaterialTable The material table methodToolTable The tool table method-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-