PartObjectColorSelection Enumeration¶
NXOpen.Preferences.PartObject.ColorSelection is an alias for NXOpen.Preferences.PartObjectColorSelection
-
class
NXOpen.Preferences.
PartObjectColorSelection
¶ Bases:
object
Describes whether color of object is not changed or it is default color or it is defined by user
Enum Members
Enum Member Enum Member Description NoChange No ChangeDefaultColor Default ColorColor User Defined Color-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-