PartModeling Class¶
-
class
NXOpen.Preferences.
PartModeling
¶ Bases:
object
Represents the set of Modeling preferences applicable to part
To obtain an instance of this class, refer to
NXOpen.Preferences.PartPreferences
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
AngleToleranceData | Returns or sets the angle tolerance data. |
C0KnotLineColor | Returns or sets the C0 knot line color |
C0KnotLineFont | Returns or sets the C0 knot line font |
C0KnotUseBodyColor | Returns or sets whether c0 knot line use body color |
C0KnotUseBodyFont | Returns or sets whether C0_knot use body font |
C1KnotLineColor | Returns or sets the C1 knot line color |
C1KnotLineFont | Returns or sets the C1 knot line font |
C1KnotUseBodyColor | Returns or sets whether c1 knot line use body color |
C1KnotUseBodyFont | Returns or sets whether C1_knot use body font |
C2KnotLineColor | Returns or sets the C2 knot line color |
C2KnotLineFont | Returns or sets the C2 knot line font |
C2KnotUseBodyColor | Returns or sets whether c2 knot line use body color |
C2KnotUseBodyFont | Returns or sets whether C2_knot use body font |
CurveCurvatureDisplay | Returns or sets the curve curvature display. |
CurveCurvatureShowCap | Returns or sets the curve curvature display show cap line |
CurveCurvatureStyle | Returns or sets the curve curvature display style |
CutViewUpdateDelayed | Returns or sets the state of the cut view delay update flag. |
Density | Returns or sets the density. |
DensityUnit | Returns or sets the density unit |
DisplayCurveCurvatureOutside | Returns or sets the curve curvature display style to show it on the inside/outside of the curve |
DistanceToleranceData | Returns or sets the modeling distance tolerance data. |
GridLineColor | Returns or sets the grid line color |
GridLineFont | Returns or sets the grid line font |
GridLinesUCount | Returns or sets the U count for grid lines. |
GridLinesVCount | Returns or sets the V count for grid lines. |
GridResolution | Returns or sets the grid resolution. |
GridUseBodyColor | Returns or sets whether grid line use body color |
GridUseBodyFont | Returns or sets whether grid use body font |
OptimizeCurve | Returns or sets the optimize curve flag |
OptimizeCurveToleranceFactor | Returns or sets the optimize curve tolerance factor |
Methods¶
Method | Description |
---|---|
GetHistoryMode | Returns whether the part is in History or History-Free mode. |
SetHistoryFreeMode | Changes the modeling mode to History-Free Modeling. |
SetHistoryMode | Changes the modeling mode to History Modeling. |
Enumerations¶
PartModelingCurveCurvatureDisplayType Enumeration | Describes whether the curve curvature display is Curvature Comb or radius of Curvature Comb |
PartModelingDensityUnitType Enumeration | Describes the units available for representing density |
PartModelingGridKnotLineFontType Enumeration | the available font for grid/knot line |
PartModelingGridResolutionType Enumeration | Describes all available grid resolutions for selection |
Property Detail¶
AngleToleranceData¶
-
PartModeling.
AngleToleranceData
¶ Returns or sets the angle tolerance data.
Angle tolerance is the maximum allowable angle between the surface normals at corresponding points, or the maximum allowable angle between curve tangent vectors at corresponding points. This value can be read from any part but can only be set when the part owning these preferences is the work part.
-------------------------------------
Getter Method
Signature
AngleToleranceData()
Returns: Return type: float New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleToleranceData(angleTolData)
Parameters: angleTolData (float) – New in version NX3.0.0.
License requirements: None.
C0KnotLineColor¶
-
PartModeling.
C0KnotLineColor
¶ Returns or sets the C0 knot line color
-------------------------------------
Getter Method
Signature
C0KnotLineColor()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
C0KnotLineColor(knotLineColor)
Parameters: knotLineColor (int) – New in version NX5.0.0.
License requirements: None.
C0KnotLineFont¶
-
PartModeling.
C0KnotLineFont
¶ Returns or sets the C0 knot line font
-------------------------------------
Getter Method
Signature
C0KnotLineFont()
Returns: Return type: NXOpen.Preferences.PartModelingGridKnotLineFontType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
C0KnotLineFont(knotLineFont)
Parameters: knotLineFont ( NXOpen.Preferences.PartModelingGridKnotLineFontType
) –New in version NX5.0.0.
License requirements: None.
C0KnotUseBodyColor¶
-
PartModeling.
C0KnotUseBodyColor
¶ Returns or sets whether c0 knot line use body color
-------------------------------------
Getter Method
Signature
C0KnotUseBodyColor()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
C0KnotUseBodyColor(useBodyColor)
Parameters: useBodyColor (bool) – New in version NX5.0.0.
License requirements: None.
C0KnotUseBodyFont¶
-
PartModeling.
C0KnotUseBodyFont
¶ Returns or sets whether C0_knot use body font
-------------------------------------
Getter Method
Signature
C0KnotUseBodyFont()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
C0KnotUseBodyFont(useBodyFont)
Parameters: useBodyFont (bool) – New in version NX5.0.0.
License requirements: None.
C1KnotLineColor¶
-
PartModeling.
C1KnotLineColor
¶ Returns or sets the C1 knot line color
-------------------------------------
Getter Method
Signature
C1KnotLineColor()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
C1KnotLineColor(knotLineColor)
Parameters: knotLineColor (int) – New in version NX5.0.0.
License requirements: None.
C1KnotLineFont¶
-
PartModeling.
C1KnotLineFont
¶ Returns or sets the C1 knot line font
-------------------------------------
Getter Method
Signature
C1KnotLineFont()
Returns: Return type: NXOpen.Preferences.PartModelingGridKnotLineFontType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
C1KnotLineFont(knotLineFont)
Parameters: knotLineFont ( NXOpen.Preferences.PartModelingGridKnotLineFontType
) –New in version NX5.0.0.
License requirements: None.
C1KnotUseBodyColor¶
-
PartModeling.
C1KnotUseBodyColor
¶ Returns or sets whether c1 knot line use body color
-------------------------------------
Getter Method
Signature
C1KnotUseBodyColor()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
C1KnotUseBodyColor(useBodyColor)
Parameters: useBodyColor (bool) – New in version NX5.0.0.
License requirements: None.
C1KnotUseBodyFont¶
-
PartModeling.
C1KnotUseBodyFont
¶ Returns or sets whether C1_knot use body font
-------------------------------------
Getter Method
Signature
C1KnotUseBodyFont()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
C1KnotUseBodyFont(useBodyFont)
Parameters: useBodyFont (bool) – New in version NX5.0.0.
License requirements: None.
C2KnotLineColor¶
-
PartModeling.
C2KnotLineColor
¶ Returns or sets the C2 knot line color
-------------------------------------
Getter Method
Signature
C2KnotLineColor()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
C2KnotLineColor(knotLineColor)
Parameters: knotLineColor (int) – New in version NX5.0.0.
License requirements: None.
C2KnotLineFont¶
-
PartModeling.
C2KnotLineFont
¶ Returns or sets the C2 knot line font
-------------------------------------
Getter Method
Signature
C2KnotLineFont()
Returns: Return type: NXOpen.Preferences.PartModelingGridKnotLineFontType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
C2KnotLineFont(knotLineFont)
Parameters: knotLineFont ( NXOpen.Preferences.PartModelingGridKnotLineFontType
) –New in version NX5.0.0.
License requirements: None.
C2KnotUseBodyColor¶
-
PartModeling.
C2KnotUseBodyColor
¶ Returns or sets whether c2 knot line use body color
-------------------------------------
Getter Method
Signature
C2KnotUseBodyColor()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
C2KnotUseBodyColor(useBodyColor)
Parameters: useBodyColor (bool) – New in version NX5.0.0.
License requirements: None.
C2KnotUseBodyFont¶
-
PartModeling.
C2KnotUseBodyFont
¶ Returns or sets whether C2_knot use body font
-------------------------------------
Getter Method
Signature
C2KnotUseBodyFont()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
C2KnotUseBodyFont(useBodyFont)
Parameters: useBodyFont (bool) – New in version NX5.0.0.
License requirements: None.
CurveCurvatureDisplay¶
-
PartModeling.
CurveCurvatureDisplay
¶ Returns or sets the curve curvature display.
-------------------------------------
Getter Method
Signature
CurveCurvatureDisplay()
Returns: Return type: NXOpen.Preferences.PartModelingCurveCurvatureDisplayType
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CurveCurvatureDisplay(curveCurvatureDisplay)
Parameters: curveCurvatureDisplay ( NXOpen.Preferences.PartModelingCurveCurvatureDisplayType
) –New in version NX3.0.0.
License requirements: None.
CurveCurvatureShowCap¶
-
PartModeling.
CurveCurvatureShowCap
¶ Returns or sets the curve curvature display show cap line
-------------------------------------
Getter Method
Signature
CurveCurvatureShowCap()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CurveCurvatureShowCap(newShowCap)
Parameters: newShowCap (bool) – New in version NX5.0.0.
License requirements: None.
CurveCurvatureStyle¶
-
PartModeling.
CurveCurvatureStyle
¶ Returns or sets the curve curvature display style
-------------------------------------
Getter Method
Signature
CurveCurvatureStyle()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CurveCurvatureStyle(newStyle)
Parameters: newStyle (int) – New in version NX5.0.0.
License requirements: None.
CutViewUpdateDelayed¶
-
PartModeling.
CutViewUpdateDelayed
¶ Returns or sets the state of the cut view delay update flag.
-------------------------------------
Getter Method
Signature
CutViewUpdateDelayed()
Returns: The current state of the delay update flag. Return type: bool New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutViewUpdateDelayed(isDelayed)
Parameters: isDelayed (bool) – The new state of the delay update flag. New in version NX4.0.0.
License requirements: None.
Density¶
-
PartModeling.
Density
¶ Returns or sets the density.
The value used to set this property must be in the units of the density units preference (that is, the value of
NXOpen.Preferences.PartModeling.DensityUnit
). Likewise, the density returned by this property is in the units of the density units preference.-------------------------------------
Getter Method
Signature
Density()
Returns: Return type: float New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Density(density)
Parameters: density (float) – New in version NX3.0.0.
License requirements: None.
DensityUnit¶
-
PartModeling.
DensityUnit
¶ Returns or sets the density unit
-------------------------------------
Getter Method
Signature
DensityUnit()
Returns: Return type: NXOpen.Preferences.PartModelingDensityUnitType
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DensityUnit(densityUnit)
Parameters: densityUnit ( NXOpen.Preferences.PartModelingDensityUnitType
) –New in version NX3.0.0.
License requirements: None.
DisplayCurveCurvatureOutside¶
-
PartModeling.
DisplayCurveCurvatureOutside
¶ Returns or sets the curve curvature display style to show it on the inside/outside of the curve
-------------------------------------
Getter Method
Signature
DisplayCurveCurvatureOutside()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayCurveCurvatureOutside(displayOutside)
Parameters: displayOutside (bool) – New in version NX5.0.0.
License requirements: None.
DistanceToleranceData¶
-
PartModeling.
DistanceToleranceData
¶ Returns or sets the modeling distance tolerance data.
This tolerance value is used throughout the Modeling application, such as for creating swept and revolved solid bodies and sectioning solid bodies. For example, when creating sheet bodies, the distance tolerance specifies the maximum allowable distance between corresponding points on the original surface and the resulting B-surface. This value can be read from any part but can only be set when the part owning these preferences is the work part.
-------------------------------------
Getter Method
Signature
DistanceToleranceData()
Returns: Return type: float New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceToleranceData(distTolData)
Parameters: distTolData (float) – New in version NX3.0.0.
License requirements: None.
GridLineColor¶
-
PartModeling.
GridLineColor
¶ Returns or sets the grid line color
-------------------------------------
Getter Method
Signature
GridLineColor()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GridLineColor(gridLineColor)
Parameters: gridLineColor (int) – New in version NX5.0.0.
License requirements: None.
GridLineFont¶
-
PartModeling.
GridLineFont
¶ Returns or sets the grid line font
-------------------------------------
Getter Method
Signature
GridLineFont()
Returns: Return type: NXOpen.Preferences.PartModelingGridKnotLineFontType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GridLineFont(gridLineFont)
Parameters: gridLineFont ( NXOpen.Preferences.PartModelingGridKnotLineFontType
) –New in version NX5.0.0.
License requirements: None.
GridLinesUCount¶
-
PartModeling.
GridLinesUCount
¶ Returns or sets the U count for grid lines.
It is the number of grid curves in the U direction of the faces of the body
-------------------------------------
Getter Method
Signature
GridLinesUCount()
Returns: Return type: int New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GridLinesUCount(gridLineUCount)
Parameters: gridLineUCount (int) – New in version NX3.0.0.
License requirements: None.
GridLinesVCount¶
-
PartModeling.
GridLinesVCount
¶ Returns or sets the V count for grid lines.
It is the number of grid curves in the V direction of the faces of the body
-------------------------------------
Getter Method
Signature
GridLinesVCount()
Returns: Return type: int New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GridLinesVCount(gridLineVCount)
Parameters: gridLineVCount (int) – New in version NX3.0.0.
License requirements: None.
GridResolution¶
-
PartModeling.
GridResolution
¶ Returns or sets the grid resolution.
The six options, None, Coarse, Standard, Fine, Extra Fine and Ultra Fine, produce a grid that is respectively more detailed. The None option shows no grid at all in wireframe mode.
-------------------------------------
Getter Method
Signature
GridResolution()
Returns: Return type: NXOpen.Preferences.PartModelingGridResolutionType
New in version NX3.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GridResolution(gridResolution)
Parameters: gridResolution ( NXOpen.Preferences.PartModelingGridResolutionType
) –New in version NX3.0.0.
License requirements: None.
GridUseBodyColor¶
-
PartModeling.
GridUseBodyColor
¶ Returns or sets whether grid line use body color
-------------------------------------
Getter Method
Signature
GridUseBodyColor()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GridUseBodyColor(useBodyColor)
Parameters: useBodyColor (bool) – New in version NX5.0.0.
License requirements: None.
GridUseBodyFont¶
-
PartModeling.
GridUseBodyFont
¶ Returns or sets whether grid use body font
-------------------------------------
Getter Method
Signature
GridUseBodyFont()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GridUseBodyFont(useBodyFont)
Parameters: useBodyFont (bool) – New in version NX5.0.0.
License requirements: None.
OptimizeCurve¶
-
PartModeling.
OptimizeCurve
¶ Returns or sets the optimize curve flag
-------------------------------------
Getter Method
Signature
OptimizeCurve()
Returns: Flag indicating whether Optimized Curve should be performed Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OptimizeCurve(optimizeCurve)
Parameters: optimizeCurve (bool) – Flag indicating whether Optimized Curve should be performed New in version NX8.0.0.
License requirements: None.
OptimizeCurveToleranceFactor¶
-
PartModeling.
OptimizeCurveToleranceFactor
¶ Returns or sets the optimize curve tolerance factor
-------------------------------------
Getter Method
Signature
OptimizeCurveToleranceFactor()
Returns: Factor for performing Optimized Curve Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OptimizeCurveToleranceFactor(optimieCurveFactor)
Parameters: optimieCurveFactor (float) – Factor for performing Optimized Curve New in version NX8.0.0.
License requirements: None.
Method Detail¶
GetHistoryMode¶
-
PartModeling.
GetHistoryMode
¶ Returns whether the part is in History or History-Free mode.
Return true for History mode or false for History-Free mode.
Signature
GetHistoryMode()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
SetHistoryFreeMode¶
-
PartModeling.
SetHistoryFreeMode
¶ Changes the modeling mode to History-Free Modeling.
This will remove parameters from features in the model. Feature edit will not be available and the model will not update.
Signature
SetHistoryFreeMode()
New in version NX6.0.0.
License requirements: None.