PartAeroSheetmetal Class¶
-
class
NXOpen.Preferences.
PartAeroSheetmetal
¶ Bases:
object
Represents the NX Sheetmetal preferences applicable to part
Preferences are in control of the part. They can not be created but can only be changed.
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
GetJoggleDepthThreshold | RETURNS the joggle depth threshold expression @return expression object for joggle depth threshold |
GetJoggleDistanceThreshold | RETURNS the joggle distance threshold expression @return expression object for joggle distance threshold |
GetJoggleOffsetRadius | RETURNS the joggle offset radius expression @return expression object for joggle offset radius |
GetJoggleStationaryRadius | RETURNS the joggle stationary radius expression @return expression object for joggle stationary radius |
SetJoggleDepthThreshold | THE joggle depth threshold value |
SetJoggleDistanceThreshold | THE joggle distance threshold value |
SetJoggleOffsetRadius | The joggle offset radius value |
SetJoggleStationaryRadius | THE joggle stationary radius value string |
Method Detail¶
GetJoggleDepthThreshold¶
-
PartAeroSheetmetal.
GetJoggleDepthThreshold
¶ RETURNS the joggle depth threshold expression
Signature
GetJoggleDepthThreshold()
Returns: expression object for joggle depth threshold Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”)
GetJoggleDistanceThreshold¶
-
PartAeroSheetmetal.
GetJoggleDistanceThreshold
¶ RETURNS the joggle distance threshold expression
Signature
GetJoggleDistanceThreshold()
Returns: expression object for joggle distance threshold Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”)
GetJoggleOffsetRadius¶
-
PartAeroSheetmetal.
GetJoggleOffsetRadius
¶ RETURNS the joggle offset radius expression
Signature
GetJoggleOffsetRadius()
Returns: expression object for joggle offset radius Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”)
GetJoggleStationaryRadius¶
-
PartAeroSheetmetal.
GetJoggleStationaryRadius
¶ RETURNS the joggle stationary radius expression
Signature
GetJoggleStationaryRadius()
Returns: expression object for joggle stationary radius Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”)
SetJoggleDepthThreshold¶
-
PartAeroSheetmetal.
SetJoggleDepthThreshold
¶ THE joggle depth threshold value
Signature
SetJoggleDepthThreshold(updateModel, depthThreshold)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- depthThreshold (str) – default joggle depth threshold value NOTE: The full Unicode character set is not supported for this parameter.
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”)
SetJoggleDistanceThreshold¶
-
PartAeroSheetmetal.
SetJoggleDistanceThreshold
¶ THE joggle distance threshold value
Signature
SetJoggleDistanceThreshold(updateModel, distanceThreshold)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- distanceThreshold (str) – default joggle depth threshold value NOTE: The full Unicode character set is not supported for this parameter.
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”)
SetJoggleOffsetRadius¶
-
PartAeroSheetmetal.
SetJoggleOffsetRadius
¶ The joggle offset radius value
Signature
SetJoggleOffsetRadius(updateModel, offsetRadius)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- offsetRadius (str) – default joggle offset radius value NOTE: The full Unicode character set is not supported for this parameter.
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”)
SetJoggleStationaryRadius¶
-
PartAeroSheetmetal.
SetJoggleStationaryRadius
¶ THE joggle stationary radius value string
Signature
SetJoggleStationaryRadius(updateModel, stationaryRadius)
Parameters: - updateModel (bool) – Specifies whether the solid model be recomputed immediately
- stationaryRadius (str) – default joggle stationary radius value NOTE: The full Unicode character set is not supported for this parameter.
New in version NX4.0.0.
License requirements: aero_sheet_metal (“Aerospace Sheet Metal”)